STM32Cube Software Examples ¶
STM32Cube Software Examples demonstrate how to use the STM32 microcontrollers with the STM32Cube ecosystem.
They run on the STM32 development boards and Discovery kits.
Build, flash, and run an example.
Browse an example and learn from it.
Modify an example with an IDE.
Troubleshoot and example if something goes wrong.
Porting an example from a board to another board.
Get more added-value with the STM32Cube ecosystem.
To get more information about STM32, visit the STM32 MCU Developer Zone and the STM32Cube ecosystem page.
Note
This user manual is dedicated to the HAL2 based STM32Cube offer.
Refer to the appropriate application note for any HAL1 based product, for example, the AN4726 for STM32L4 Series and STM32L4+ Series .