HAL_SHA256_ALT

MBEDTLS IMPLEMENTATION HAL SHA256 ALT FUNCTIONS

group MBEDTLS_IMPLEMENTATION_HAL_SHA256_ALT_FUNCTIONS

Public API functions for HAL SHA256 alternate implementation.

Functions

void mbedtls_sha256_init ( mbedtls_sha256_context * ctx )
void mbedtls_sha256_free ( mbedtls_sha256_context * ctx )
void mbedtls_sha256_clone ( mbedtls_sha256_context * dst , const mbedtls_sha256_context * src )
int mbedtls_sha256_starts ( mbedtls_sha256_context * ctx , int is224 )
int mbedtls_sha256_update ( mbedtls_sha256_context * ctx , const unsigned char * input , size_t ilen )
int mbedtls_sha256_finish ( mbedtls_sha256_context * ctx , unsigned char * output )

MBEDTLS IMPLEMENTATION HAL SHA256 TYPES

group MBEDTLS_IMPLEMENTATION_HAL_SHA256_TYPES

This file contains SHA-224 and SHA-256 definitions and functions based on STM32 HASH hardware crypto accelerator.

The Secure Hash Algorithms 224 and 256 (SHA-224 and SHA-256) cryptographic hash functions are defined in FIPS 180-4: Secure Hash Standard (SHS) .

SHA-256 context structure.

The structure is used both for SHA-256 and for SHA-224 checksum calculations. The choice between these two is made in the call to mbedtls_sha256_starts_ret().

struct mbedtls_sha256_context
#include <hal_sha256_alt.h>

Public Members

int is224

0 = use SHA256, 1 = use SHA224

uint32_t output_size_byte

output length

cmox_hash_handle_t * hash_ctx

Hash ctx

cmox_sha256_handle_t sha256_ctx

Sha256 ctx

cmox_sha224_handle_t sha224_ctx

Sha224 ctx

size_t dig_len

Digest len generate by STCryptoLib

uint8_t is224

1 if sha224, 0 otherwise