Getting started with STM32Cube MCU Package for STM32C5 series

This is the documentation for the STM32C5 MCU Package, version 2.1.0. This is part of the STM32Cube ecosystem.

What is a STM32Cube MCU Package?

STM32Cube MCU Package is an STM32Cube Software Package for a given series of STM32 microcontrollers.

It is a set of embedded software drivers, libraries and examples from the STM32Cube embedded software offer. This set of software helps developers create applications for STM32 microcontrollers.

STM32Cube MCU Package is designed to be used with a set of proposed IDEs as well as STM32CubeMX2.

Download STM32Cube MCU Package from STM32 Package Creator or STMicroelectronics GitHub.

How to use this software package?

Package content overview icon
Package content

Software components are at the heart of the STM32Cube MCU Package.

Package content
Environment setup icon
Environment setup

Minimal setup to use the STM32Cube MCU Package.

Environment setup
Run examples icon
Run examples

Example projects put the software components into action.

Run examples

Note

This document focuses on the HAL2-based STM32Cube offer.

For any HAL1-based product, more detailed information is available in STM32Cube MCU & MPU packages.