Release Notes ¶
Purpose ¶
STM32Cube enables developers to achieve design success. With a comprehensive suite of professional development tools and embedded software components, STM32Cube allows developers to differentiate products, streamline design cycles, and reduce costs. STM32Cube ecosystem supports all design steps, including selection, configuration, development, debugging, programming, and monitoring.
The STM32Cube embedded software offer provides ready-to-use software components that can be added to a project. It includes STM32 peripheral driver APIs with two levels of abstraction, middleware, board drivers, and examples. There are several distribution channels, including the STM32CubeMX2 tool, the ST website, and GitHub. All embedded software comes with enhanced online documentation, with flowcharts and user sequences.
More detailed documentation is available at STM32C5xx HAL Drivers online documentation
Update History ¶
2.1.0 / 12-June-2026 ¶
Main changes ¶
Second Official release of STM32C5xx HAL Drivers ¶
Contents ¶
HAL/LL Drivers are available for all peripherals:
System : CORTEX, CRS, DBGMCU, DMA (Q), ICACHE, IWDG, PWR, RCC, RTC, SBS, WWDG
I/O : EXTI, GPIO
Analog : ADC, COMP, DAC, OPAMP
Timers : TIM, LPTIM
Connectivity : FDCAN, I2C, I3C, SMARTCARD, SMBUS, I2S, SPI, UART, LPUART, USART, USB (HCD/PCD), ETH
Security : AES, CCB, HASH, PKA, RNG, TAMP
Computing : CORDIC, CRC
Memory : FLASH, RAMCFG, XSPI (DLYB)
Common : OS, Timebases, Templates
Utils are available for FDCAN, I2C, I3C peripherals.
HAL/LL Drivers updates
HAL/LL CORDIC
Add HAL_CORDIC_GetInstance() and HAL_CORDIC_GetLLInstance() functions
HAL/LL ICACHE
Add HAL_ICACHE_GetInstance() and HAL_ICACHE_GetLLInstance() functions
HAL GPIO
Add HAL_GPIO_GetLLInstance() function
Update HAL_GPIO_AFn_XXX alternate function definitions to align with the reference manual. Keep the old definitions as compatibility aliases.
HAL HCD
Add HAL_HCD_RegisterChannelAbortTransferCallback() and HAL_HCD_ChannelAbortTransferCallback() functions
Remove High-Speed and ULPI-related public definitions that do not apply to STM32C5 supported devices
HAL LPTIM
Remove HAL_LPTIM_CompareMatchHalfCpltCallback() prototype because LPTIM peripheral does not support it
HAL PCD
Add HAL_PCD_RegisterEndpointAbortTransferCallback() and HAL_PCD_EndpointAbortTransferCallback() functions
Remove High-Speed and ULPI-related public definitions that do not apply to STM32C5 supported devices
LL TIM
Apply naming changes to remove duplication in functions name of LL_TIM_POSITION_BRK_SOURCE(), LL_TIM_GET_CHANNEL_INDEX(), LL_TIM_CALC_DTS(). Keep the old definitions as compatibility aliases.
Development toolchains and compilers ¶
IAR Embedded Workbench for ARM (EWARM) toolchain V9.60.3 + ST-LINK
MDK-ARM Keil uVision V5.42
STM32CubeIDE for Visual Studio Code (GCC13 compiler)
STM32CubeMX2 V1.0.0
Supported devices and boards ¶
STM32C551xx, STM32C552xx, STM32C562xx devices
STM32C531xx, STM32C532xx, STM32C542xx devices
STM32C591xx, STM32C593xx, STM32C5A3xx devices
NUCLEO-C562RE (RevB02), NUCLEO-C542RC (RevB02), NUCLEO-C5A3ZG (RevB02) boards
Known limitations ¶
HAL ETH
PTP, hardware timestamping, MAC VLAN tagging and advanced MAC filtering features are not supported in this driver version and will be considered for a future release.
HAL I2C
As defined by MIPI, I2C stretch mode is not supported in I3C communication.
HAL I2S
Using the -Oz optimization in ARMCC6.24.0 may reorder peripheral memory accesses causing initialization and execution issues in HAL I2S driver.
HAL I3C
Acknowledgement issue is observed after 2 consecutive aborts (interrupt race condition).
Backward compatibility ¶
None
Dependencies ¶
STM32C5xx DFP 2.1.0
2.0.0 / 13-March-2026 ¶
Main changes ¶
First Official release of STM32C5xx HAL Drivers ¶
Contents ¶
HAL/LL Drivers are available for all peripherals:
System : CORTEX, CRS, DBGMCU, DMA (Q), ICACHE, IWDG, PWR, RCC, RTC, SBS, WWDG
I/O : EXTI, GPIO
Analog : ADC, COMP, DAC, OPAMP
Timers : TIM, LPTIM
Connectivity : FDCAN, I2C, I3C, SMARTCARD, SMBUS, I2S, SPI, UART, LPUART, USART, USB (HCD/PCD), ETH
Security : AES, CCB, HASH, PKA, RNG, TAMP
Computing : CORDIC, CRC
Memory : FLASH, RAMCFG, XSPI (DLYB)
Common : OS, Timebases, Templates
Utils are available for FDCAN, I2C, I3C peripherals.
Development toolchains and compilers ¶
IAR Embedded Workbench for ARM (EWARM) toolchain V9.60.3 + ST-LINK
MDK-ARM Keil uVision V5.42
STM32CubeIDE for Visual Studio Code (GCC13 compiler)
STM32CubeMX2 V1.0.0
Supported devices and boards ¶
STM32C551xx, STM32C552xx, STM32C562xx devices
STM32C531xx, STM32C532xx, STM32C542xx devices
STM32C591xx, STM32C593xx, STM32C5A3xx devices
NUCLEO-C562RE, NUCLEO-C542RC, NUCLEO-C5A3ZG boards
Known limitations ¶
HAL ETH
PTP, hardware timestamping, MAC VLAN tagging and advanced MAC filtering features are not supported in this driver version and will be considered for a future release.
HAL HASH
When using HAL_HASH_Update_DMA(), no interrupt is triggered when the input is smaller than the DMA block size (4 words).
When using HAL_HASH_Update_IT(), no interrupt is triggered when the input is smaller than the block size.
HAL I2C
As defined by MIPI, I2C stretch mode is not supported in I3C communication.
HAL I2S
Using the -Oz optimization in ARMCC6.24.0 may reorder peripheral memory accesses causing initialization and execution issues in HAL I2S driver.
HAL I3C
Acknowledgement issue is observed after 2 consecutive aborts (interrupt race condition).
Backward compatibility ¶
None
Dependencies ¶
STM32C5xx DFP 2.0.0