Known issues ¶
Missing Windows ST-Link driver for STM32CubeIDE for Visual Studio Code ¶
Issue : On a new Windows 11 PC, users who install Visual Studio Code and the STM32CubeIDE extension may experience issues detecting STM32 boards with ST-Link v2 or v2.1.
Symptoms :
No device appears in the STM32Cube Devices and Boards webview.
No device is detected with ST-Linkupgrade.exe.
Complex project creation ¶
Issue : Complex projects created using the empty project feature are incorrectly set up as non-complex.
Example : H7 dual-core projects are created as mono-core.
Cube command not available on Windows with Git Bash ¶
Issue : The cube command is not available when using Git Bash on Windows.
Workaround : Windows users must manually configure their environment, for example, by editing .bashrc or Visual Studio Code settings.
STLINK-V3 not working with macOS M architecture ¶
Issue : STLINK-V3 devices do not function properly on macOS with M architecture.
Workaround : Use a USB hub instead of a Type-C to Type-C cable.
libncurses5 dependency on Linux ¶
Issue : Debug sessions may fail due to a missing libncurses5 dependency.
Note : Fixed. Dedicated STM32Cube bundles serve GNU Tools for STM32 assets. Update if possible.
Workarounds :
Ubuntu 22.04: Install with:
sudo apt-get install libncurses5Ubuntu 24.04: - Use the following commands to manually install the library:
wget http://archive.ubuntu.com/ubuntu/pool/universe/n/ncurses/libtinfo5_6.4-2_amd64.deb && sudo dpkg -i libtinfo5_6.4-2_amd64.deb && rm -f libtinfo5_6.4-2_amd64.deb wget http://archive.ubuntu.com/ubuntu/pool/universe/n/ncurses/libncurses5_6.4-2_amd64.deb && sudo dpkg -i libncurses5_6.4-2_amd64.deb && rm -f libncurses5_6.4-2_amd64.deb
Fedora 41: Install the necessary libraries with:
sudo dnf install ncurses-compat-libs
Clangd indexing dependency on zstd Library on macOS ¶
Issue : Clangd indexing does not work on macOS due to a missing zstd library.
Workaround : Install Homebrew and then run:
brew install zstd
CMake error with Visual Studio Code installed via the Snap Store on Ubuntu ¶
Issue : CMake fails to discover projects when Microsoft Visual Studio Code is installed via the Snap Store.
Workaround : Install Visual Studio Code using a different method, for example, download the .deb package directly from the official website or use an alternative package manager such as apt or flatpak .
Using J-Link to debug on macOS ¶
Issue : Attempting to debug causes the error “JLinkConfig” is damaged and can’t be opened. You should move it to the Bin.”
Workaround : Go to the Privacy & Security setting and click Open Anyway for the JLinkConfig.app application.
Creating an empty project while offline ¶
Issue : When creating an empty project while offline, a faulty project is generated.
Workaround : Go online when creating the project. It is then safe to go back to offline mode.