1 STM32Cube overview ¶
STM32Cube is an STMicroelectronics original initiative to improve designer productivity significantly by reducing development effort, time, and cost. STM32Cube covers the whole portfolio of STM32 devices, based on 32-bit Arm ® Cortex ®(a) cores.
STM32Cube includes:
A set of user-friendly software development tools to cover project development from conception to realization, among which are:
STM32CubeMX, a graphical software configuration tool that allows the automatic generation of C initialization code using graphical wizards
STM32CubeIDE, an Eclipse®-based IDE, providing code edition, compilation, programming, and debugging capabilities
STM32CubeCLT, an all-in-one command-line development toolset with code compilation, board programming, and debug features
STM32CubeIDE for Visual Studio Code (STM32VSCode), a complete IDE based on VS Code® platform
STM32CubeProgrammer (STM32CubeProg), a programming tool available in graphical and command-line versions
STM32CubeMonitor (STM32CubeMonitor, STM32CubeMonPwr, STM32CubeMonRF, STM32CubeMonUCPD), powerful monitoring tools to finetune the behavior and performance of STM32 applications in real time
STM32CubeWiSE (STM32CubeWiSEcg, STM32CubeWiSEre), graphical tools designed to evaluate and test the capabilities of sub-GHz radios and protocols
A set of user-friendly software development tools to cover project development from conception to realization, among which are:
STM32CubeMX, a graphical software configuration tool that allows the automatic generation of C initialization code using graphical wizards
STM32CubeIDE, an all-in-one development tool with peripheral configuration, code generation, code compilation, and debug features
STM32CubeCLT, an all-in-one command-line development toolset with code compilation, board programming, and debug features
STM32CubeProgrammer (STM32CubeProg), a programming tool available in graphical and command-line versions
*Note: Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries or affiliates) in the US and/or elsewhere.
*The Arm word and logo are trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere. All rights reserved.
STM32CubeMonitor (STM32CubeMonitor, STM32CubeMonPwr, STM32CubeMonRF, STM32CubeMonUCPD), powerful monitoring tools to fine-tune the behavior and performance of STM32 applications in real time
STM32Cube MCU and MPU Packages, comprehensive embedded-software platforms specific to each microcontroller and microprocessor series (such as STM32CubeH5 for the STM32H5 series), which include:
STM32Cube hardware abstraction layer (HAL), ensuring maximized portability across the STM32 portfolio
STM32Cube low-layer APIs, ensuring the best performance and footprints with a high degree of user control over hardware
A consistent set of middleware components, such as ThreadX, FileX / LevelX, NetX Duo, USBX, USB-PD, mbed-crypto, secure manager API, MCUboot, and OpenBL
All embedded software utilities with full sets of peripheral and applicative examples
STM32Cube Expansion Packages, which contain embedded software components that complement the functionalities of the STM32Cube MCU and MPU Packages with:
Middleware extensions and applicative layers
Examples running on some specific STMicroelectronics development boards