Release fixes

Main fixed issues for 6.19.0

Main fixed issues for 6.19.0

ID

Summary

TMX1-58679

When generating code for USB_OTG_FS on STM32H743, STM32CubeMX generated an incorrect alternate function assignment (GPIO_AF10_OTG1_FS instead of GPIO_AF10_OTG2_FS).

STM32CubeMX version 6.19.0 fixes this issue.

TMX1-57469

When RTC clock source HSE/48 was selected on STM32H5 devices, incorrect code could be generated.

STM32CubeMX version 6.19.0 fixes this issue.

TMX1-56055

When UART was configured in Single Wire Mode using LL drivers, GPIO configuration could be generated incorrectly.

STM32CubeMX version 6.19.0 fixes this issue.

TMX1-37036

When HSE or LSE was configured in Bypass mode, OSC_OUT and OSC32_OUT pins were not kept as normal GPIO pins.

STM32CubeMX version 6.19.0 fixes this issue.

TMX1-35501

When RTC Wake-Up Timer was enabled, the generated code was missing the HAL_RTCEx_SetWakeUpTimer_IT() API call.

STM32CubeMX version 6.19.0 fixes this issue.

TMX1-35462

When configuring SAI Block B as Master, the MASTER Clock No Divider option was not available.

STM32CubeMX version 6.19.0 fixes this issue.

TMX1-35028

In STM32CubeMX v6.15.0, generated configuration could cause RS485/RS232 communication failures.

STM32CubeMX version 6.19.0 fixes this issue.