HAL RAMCFG Overview

Introducing RAMCFG

group RAMCFG_Introduction

  • This introduction is under development.

Module and files

The following diagram illustrates the RAMCFG module and its associated files.

Module and files diagram

Component diagram

The following diagram illustrates the software components involved in the RAMCFG module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.

Configuration table

The following table lists the configuration defines for the HAL RAMCFG module, specifying their locations, default values, and descriptions:

group RAMCFG_Configuration_Table

Configuration inside the RAMCFG driver

Config defines

Description

Default value

Note

PRODUCT

from IDE

NA

Ex:STM32U585XX.

USE_ASSERT_DBG_PARAM

from IDE

None

Enable the parameters asserts.

USE_HAL_CHECK_PARAM

from hal_conf.h

0

Enable the parameters runtime checks.

USE_HAL_RAMCFG_MODULE

from hal_conf.h

1

Enable the HAL RAMCFG module.