HAL WWDG Functions ¶
Initialization and Start functions ¶
- group WWDG_Exported_Functions_Group1
-
This subsection provides a set of functions allowing to initialize and start the WWDG peripheral:
-
Call the function HAL_WWDG_Init() to initialize the WWDG handle and associate an instance.
-
Call the function HAL_WWDG_Start() to start the WWDG according to the parameters provided by the user.
Functions
-
hal_status_t
HAL_WWDG_Init
(
hal_wwdg_handle_t
*
hwwdg
,
hal_wwdg_t
instance
)
¶
-
Initialize the WWDG according to the associated handle.
Warning
In case of starting WWDG in Hardware mode, make sure that USE_HAL_WWDG_HARDWARE_START is aligned with the WWDG_SW option byte.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
instance – WWDG instance.
-
- Return values :
-
-
HAL_OK – HAL operation completed successfully.
-
HAL_INVALID_PARAM – HAL invalid parameter.
-
-
hal_status_t
HAL_WWDG_Start
(
hal_wwdg_handle_t
*
hwwdg
,
uint32_t
min_time
,
uint32_t
max_time
,
uint32_t
ewi_status
)
¶
-
Start the WWDG. Before exiting the function, the watchdog counter is refreshed to have a correct time base.
Note
The default time unit is milliseconds if not specified through USE_HAL_WWDG_TIME_UNIT define.
Warning
The max_time and min_time are used to define the reload and the window values, the unit for these parameters depends on the switch USE_HAL_WWDG_TIME_UNIT.
Warning
The ewi_status must be set to zero when Early Wakeup Interrupt feature is not used.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
min_time – Minimum time value before refreshing is allowed.
-
max_time – Maximum time value before a WWDG reset.
-
ewi_status – Early Wakeup Interrupt activation.
-
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
- group WWDG_Exported_Functions_Group1
-
This subsection provides a set of functions allowing to initialize and start the WWDG peripheral:
-
Call the function HAL_WWDG_Init() to initialize the WWDG handle and associate an instance.
-
Call the function HAL_WWDG_Start() to start the WWDG according to the parameters provided by the user.
Functions
-
hal_status_t
HAL_WWDG_Init
(
hal_wwdg_handle_t
*
hwwdg
,
hal_wwdg_t
instance
)
-
Initialize the WWDG according to the associated handle.
Warning
In case of starting WWDG in Hardware mode, make sure that USE_HAL_WWDG_HARDWARE_START is aligned with the WWDG_SW option byte.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
instance – WWDG instance.
-
- Return values :
-
-
HAL_OK – HAL operation completed successfully.
-
HAL_INVALID_PARAM – HAL invalid parameter.
-
-
hal_status_t
HAL_WWDG_Start
(
hal_wwdg_handle_t
*
hwwdg
,
uint32_t
min_time
,
uint32_t
max_time
,
uint32_t
ewi_status
)
-
Start the WWDG. Before exiting the function, the watchdog counter is refreshed to have a correct time base.
Note
The default time unit is milliseconds if not specified through USE_HAL_WWDG_TIME_UNIT define.
Warning
The max_time and min_time are used to define the reload and the window values, the unit for these parameters depends on the switch USE_HAL_WWDG_TIME_UNIT.
Warning
The ewi_status must be set to zero when Early Wakeup Interrupt feature is not used.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
min_time – Minimum time value before refreshing is allowed.
-
max_time – Maximum time value before a WWDG reset.
-
ewi_status – Early Wakeup Interrupt activation.
-
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
- group WWDG_Exported_Functions_Group1
-
This subsection provides a set of functions allowing to initialize and start the WWDG peripheral:
-
Call the function HAL_WWDG_Init() to initialize the WWDG handle and associate an instance.
-
Call the function HAL_WWDG_Start() to start the WWDG according to the parameters provided by the user.
Functions
-
hal_status_t
HAL_WWDG_Init
(
hal_wwdg_handle_t
*
hwwdg
,
hal_wwdg_t
instance
)
-
Initialize the WWDG according to the associated handle.
Warning
In case of starting WWDG in Hardware mode, make sure that USE_HAL_WWDG_HARDWARE_START is aligned with the WWDG_SW option byte.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
instance – WWDG instance.
-
- Return values :
-
-
HAL_OK – HAL operation completed successfully.
-
HAL_INVALID_PARAM – HAL invalid parameter.
-
-
hal_status_t
HAL_WWDG_Start
(
hal_wwdg_handle_t
*
hwwdg
,
uint32_t
min_time
,
uint32_t
max_time
,
uint32_t
ewi_status
)
-
Start the WWDG. Before exiting the function, the watchdog counter is refreshed to have a correct time base.
Note
The default time unit is milliseconds if not specified through USE_HAL_WWDG_TIME_UNIT define.
Warning
The max_time and min_time are used to define the reload and the window values, the unit for these parameters depends on the switch USE_HAL_WWDG_TIME_UNIT.
Warning
The ewi_status must be set to zero when Early Wakeup Interrupt feature is not used.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
min_time – Minimum time value before refreshing is allowed.
-
max_time – Maximum time value before a WWDG reset.
-
ewi_status – Early Wakeup Interrupt activation.
-
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
IO operation function ¶
- group WWDG_Exported_Functions_Group2
-
This subsection provides a function to manage the refresh of the WWDG counter:
-
Call the function HAL_WWDG_Refresh() to reload WWDG counter with value defined in the reload register.
Functions
-
hal_status_t
HAL_WWDG_Refresh
(
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Refresh the WWDG counter.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
- group WWDG_Exported_Functions_Group2
-
This subsection provides a function to manage the refresh of the WWDG counter:
-
Call the function HAL_WWDG_Refresh() to reload WWDG counter with value defined in the reload register.
Functions
-
hal_status_t
HAL_WWDG_Refresh
(
hal_wwdg_handle_t
*
hwwdg
)
-
Refresh the WWDG counter.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
- group WWDG_Exported_Functions_Group2
-
This subsection provides a function to manage the refresh of the WWDG counter:
-
Call the function HAL_WWDG_Refresh() to reload WWDG counter with value defined in the reload register.
Functions
-
hal_status_t
HAL_WWDG_Refresh
(
hal_wwdg_handle_t
*
hwwdg
)
-
Refresh the WWDG counter.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
State function ¶
- group WWDG_Exported_Functions_Group3
-
This subsection provides a function to retrieve the state value:
-
Call the function HAL_WWDG_GetState() to retrieve the WWDG handle state.
Functions
-
hal_wwdg_state_t
HAL_WWDG_GetState
(
const
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Return the WWDG handle state.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
-
HAL_WWDG_STATE_RESET – WWDG driver not initialized and not started.
-
HAL_WWDG_STATE_IDLE – WWDG driver initialized and not started.
-
HAL_WWDG_STATE_ACTIVE – WWDG driver initialized and started.
-
-
- group WWDG_Exported_Functions_Group3
-
This subsection provides a function to retrieve the state value:
-
Call the function HAL_WWDG_GetState() to retrieve the WWDG handle state.
Functions
-
hal_wwdg_state_t
HAL_WWDG_GetState
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Return the WWDG handle state.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
-
HAL_WWDG_STATE_RESET – WWDG driver not initialized and not started.
-
HAL_WWDG_STATE_IDLE – WWDG driver initialized and not started.
-
HAL_WWDG_STATE_ACTIVE – WWDG driver initialized and started.
-
-
- group WWDG_Exported_Functions_Group3
-
This subsection provides a function to retrieve the state value:
-
Call the function HAL_WWDG_GetState() to retrieve the WWDG handle state.
Functions
-
hal_wwdg_state_t
HAL_WWDG_GetState
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Return the WWDG handle state.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
-
HAL_WWDG_STATE_RESET – WWDG driver not initialized and not started.
-
HAL_WWDG_STATE_IDLE – WWDG driver initialized and not started.
-
HAL_WWDG_STATE_ACTIVE – WWDG driver initialized and started.
-
-
Set/Get item functions ¶
- group WWDG_Exported_Functions_Group4
-
This subsection provides a set of functions to set/retrieve configuration items separately for the WWDG driver:
-
Call the function HAL_WWDG_GetMaxTime() to retrieve the current maximum time value.
-
Call the function HAL_WWDG_GetStep_us() to retrieve the current counter period.
-
Call the function HAL_WWDG_SetMinTime() to set only the Window time value.
-
Call the function HAL_WWDG_GetMinTime() to retrieve the current Window time value.
Note
The prescaler is calculated from maximum time once in the HAL_WWDG_Start() function, to avoid a change of prescaler, we did not introduce a function to set the maximum time because it can modify the prescaler and thus require to recalculate the Window. To modify the maximum time, the user must proceed with the HAL_WWDG_Start() function.
Functions
-
uint32_t
HAL_WWDG_GetMaxTime
(
const
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Get the maximum time value according to the handle instance registers.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current maximum time value.
-
uint32_t
HAL_WWDG_GetStep_us
(
const
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Get the WWDG counter period in microseconds.
Note
HAL_WWDG_GetStep_us is given as information to allow the user to calculate max_time, min_time to avoid rounded values.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current counter period value in us.
-
hal_status_t
HAL_WWDG_SetMinTime
(
hal_wwdg_handle_t
*
hwwdg
,
uint32_t
min_time
)
¶
-
Set the Window time value.
Warning
User must refresh the WWDG counter before calling this function.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
min_time – Minimum time value before refreshing is allowed.
-
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
uint32_t
HAL_WWDG_GetMinTime
(
const
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Get the Window time value according to the handler instance registers.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current Window time value.
-
- group WWDG_Exported_Functions_Group4
-
This subsection provides a set of functions to set/retrieve configuration items separately for the WWDG driver:
-
Call the function HAL_WWDG_GetMaxTime() to retrieve the current maximum time value.
-
Call the function HAL_WWDG_GetStep_us() to retrieve the current counter period.
-
Call the function HAL_WWDG_SetMinTime() to set only the Window time value.
-
Call the function HAL_WWDG_GetMinTime() to retrieve the current Window time value.
Note
The prescaler is calculated from maximum time once in the HAL_WWDG_Start() function, to avoid a change of prescaler, we did not introduce a function to set the maximum time because it can modify the prescaler and thus require to recalculate the Window. To modify the maximum time, the user must proceed with the HAL_WWDG_Start() function.
Functions
-
uint32_t
HAL_WWDG_GetMaxTime
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Get the maximum time value according to the handle instance registers.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current maximum time value.
-
uint32_t
HAL_WWDG_GetStep_us
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Get the WWDG counter period in microseconds.
Note
HAL_WWDG_GetStep_us is given as information to allow the user to calculate max_time, min_time to avoid rounded values.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current counter period value in us.
-
hal_status_t
HAL_WWDG_SetMinTime
(
hal_wwdg_handle_t
*
hwwdg
,
uint32_t
min_time
)
-
Set the Window time value.
Warning
User must refresh the WWDG counter before calling this function.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
min_time – Minimum time value before refreshing is allowed.
-
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
uint32_t
HAL_WWDG_GetMinTime
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Get the Window time value according to the handler instance registers.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current Window time value.
-
- group WWDG_Exported_Functions_Group4
-
This subsection provides a set of functions to set/retrieve configuration items separately for the WWDG driver:
-
Call the function HAL_WWDG_GetMaxTime() to retrieve the current maximum time value.
-
Call the function HAL_WWDG_GetStep_us() to retrieve the current counter period.
-
Call the function HAL_WWDG_SetMinTime() to set only the Window time value.
-
Call the function HAL_WWDG_GetMinTime() to retrieve the current Window time value.
Note
The prescaler is calculated from maximum time once in the HAL_WWDG_Start() function, to avoid a change of prescaler, we did not introduce a function to set the maximum time because it can modify the prescaler and thus require to recalculate the Window. To modify the maximum time, the user must proceed with the HAL_WWDG_Start() function.
Functions
-
uint32_t
HAL_WWDG_GetMaxTime
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Get the maximum time value according to the handle instance registers.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current maximum time value.
-
uint32_t
HAL_WWDG_GetStep_us
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Get the WWDG counter period in microseconds.
Note
HAL_WWDG_GetStep_us is given as information to allow the user to calculate max_time, min_time to avoid rounded values.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current counter period value in us.
-
hal_status_t
HAL_WWDG_SetMinTime
(
hal_wwdg_handle_t
*
hwwdg
,
uint32_t
min_time
)
-
Set the Window time value.
Warning
User must refresh the WWDG counter before calling this function.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
min_time – Minimum time value before refreshing is allowed.
-
- Return values :
-
HAL_OK – HAL operation completed successfully.
-
uint32_t
HAL_WWDG_GetMinTime
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Get the Window time value according to the handler instance registers.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
- Return values :
-
uint32_t – Current Window time value.
-
IRQ Handler/Callbacks/Register Callbacks functions ¶
- group WWDG_Exported_Functions_Group5
-
This subsection provides a set of functions allowing to register the WWDG process and callbacks:
-
The function HAL_WWDG_IRQHandler() to handle WWDG interrupts
There are two ways to use callbacks:
Override weak callback function: Call the function
HAL_WWDG_EarlyWakeupCallback()to indicate that an early interrupt is pending.
Or register callbacks user: Call the function
HAL_WWDG_RegisterEarlyWakeupCallback() to register the Early Wakeup Callback.Functions
-
void
HAL_WWDG_IRQHandler
(
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Handle WWDG interrupt request.
Note
The Early Wakeup Interrupt (EWI) can be used if specific safety operations or data logging must be performed before the actual reset is generated. The EWI interrupt is enabled by calling HAL_WWDG_Start() function with an ewi_status equals to 1. When the downcounter reaches the value 0x40, an EWI interrupt is generated and the corresponding Interrupt Service Routine (ISR) can be used to trigger specific actions (such as communications or data logging), before resetting the device.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
void
HAL_WWDG_EarlyWakeupCallback
(
hal_wwdg_handle_t
*
hwwdg
)
¶
-
WWDG Early Wakeup callback.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
hal_status_t
HAL_WWDG_RegisterEarlyWakeupCallback
(
hal_wwdg_handle_t
*
hwwdg
,
hal_wwdg_cb_t
p_callback
)
¶
-
Register the user WWDG Early Wakeup Callback.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
p_callback – pointer to the hal_wwdg_cb_t Callback function
-
- Return values :
-
-
HAL_OK – HAL operation completed successfully.
-
HAL_INVALID_PARAM – HAL invalid parameter.
-
-
- group WWDG_Exported_Functions_Group5
-
This subsection provides a set of functions allowing to register the WWDG process and callbacks:
-
The function HAL_WWDG_IRQHandler() to handle WWDG interrupts
There are two ways to use callbacks:
Override weak callback function: Call the function
HAL_WWDG_EarlyWakeupCallback()to indicate that an early interrupt is pending.
Or register callbacks user: Call the function
HAL_WWDG_RegisterEarlyWakeupCallback() to register the Early Wakeup Callback.Functions
-
void
HAL_WWDG_IRQHandler
(
hal_wwdg_handle_t
*
hwwdg
)
-
Handle WWDG interrupt request.
Note
The Early Wakeup Interrupt (EWI) can be used if specific safety operations or data logging must be performed before the actual reset is generated. The EWI interrupt is enabled by calling HAL_WWDG_Start() function with an ewi_status equals to 1. When the downcounter reaches the value 0x40, an EWI interrupt is generated and the corresponding Interrupt Service Routine (ISR) can be used to trigger specific actions (such as communications or data logging), before resetting the device.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
void
HAL_WWDG_EarlyWakeupCallback
(
hal_wwdg_handle_t
*
hwwdg
)
-
WWDG Early Wakeup callback.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
hal_status_t
HAL_WWDG_RegisterEarlyWakeupCallback
(
hal_wwdg_handle_t
*
hwwdg
,
hal_wwdg_cb_t
p_callback
)
-
Register the user WWDG Early Wakeup Callback.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
p_callback – pointer to the hal_wwdg_cb_t Callback function
-
- Return values :
-
-
HAL_OK – HAL operation completed successfully.
-
HAL_INVALID_PARAM – HAL invalid parameter.
-
-
- group WWDG_Exported_Functions_Group5
-
This subsection provides a set of functions allowing to register the WWDG process and callbacks:
-
The function HAL_WWDG_IRQHandler() to handle WWDG interrupts
There are two ways to use callbacks:
Override weak callback function: Call the function
HAL_WWDG_EarlyWakeupCallback()to indicate that an early interrupt is pending.
Or register callbacks user: Call the function
HAL_WWDG_RegisterEarlyWakeupCallback() to register the Early Wakeup Callback.Functions
-
void
HAL_WWDG_IRQHandler
(
hal_wwdg_handle_t
*
hwwdg
)
-
Handle WWDG interrupt request.
Note
The Early Wakeup Interrupt (EWI) can be used if specific safety operations or data logging must be performed before the actual reset is generated. The EWI interrupt is enabled by calling HAL_WWDG_Start() function with an ewi_status equals to 1. When the downcounter reaches the value 0x40, an EWI interrupt is generated and the corresponding Interrupt Service Routine (ISR) can be used to trigger specific actions (such as communications or data logging), before resetting the device.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
void
HAL_WWDG_EarlyWakeupCallback
(
hal_wwdg_handle_t
*
hwwdg
)
-
WWDG Early Wakeup callback.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
hal_status_t
HAL_WWDG_RegisterEarlyWakeupCallback
(
hal_wwdg_handle_t
*
hwwdg
,
hal_wwdg_cb_t
p_callback
)
-
Register the user WWDG Early Wakeup Callback.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure that contains the configuration information for the specified WWDG module.
-
p_callback – pointer to the hal_wwdg_cb_t Callback function
-
- Return values :
-
-
HAL_OK – HAL operation completed successfully.
-
HAL_INVALID_PARAM – HAL invalid parameter.
-
-
User Data Function ¶
- group WWDG_Exported_Functions_Group6
-
This subsection provides functions allowing to set user specific data to a WWDG instance:
-
HAL_WWDG_SetUserData() : Set user data in handler.
-
HAL_WWDG_GetUserData() : Get user data from handler.
Functions
-
void
HAL_WWDG_SetUserData
(
hal_wwdg_handle_t
*
hwwdg
,
const
void
*
p_user_data
)
¶
-
Store User Data pointer into the handle.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure which contains the WWDG instance.
-
p_user_data – Pointer to the user data.
-
-
const
void
*
HAL_WWDG_GetUserData
(
const
hal_wwdg_handle_t
*
hwwdg
)
¶
-
Retrieve User Data pointer from the handle.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure which contains the WWDG instance.
- Return values :
-
Pointer – to the user data.
-
- group WWDG_Exported_Functions_Group6
-
This subsection provides functions allowing to set user specific data to a WWDG instance:
-
HAL_WWDG_SetUserData() : Set user data in handler.
-
HAL_WWDG_GetUserData() : Get user data from handler.
Functions
-
void
HAL_WWDG_SetUserData
(
hal_wwdg_handle_t
*
hwwdg
,
const
void
*
p_user_data
)
-
Store User Data pointer into the handle.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure which contains the WWDG instance.
-
p_user_data – Pointer to the user data.
-
-
const
void
*
HAL_WWDG_GetUserData
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Retrieve User Data pointer from the handle.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure which contains the WWDG instance.
- Return values :
-
Pointer – to the user data.
-
- group WWDG_Exported_Functions_Group6
-
This subsection provides functions allowing to set user specific data to a WWDG instance:
-
HAL_WWDG_SetUserData() : Set user data in handler.
-
HAL_WWDG_GetUserData() : Get user data from handler.
Functions
-
void
HAL_WWDG_SetUserData
(
hal_wwdg_handle_t
*
hwwdg
,
const
void
*
p_user_data
)
-
Store User Data pointer into the handle.
- Parameters :
-
-
hwwdg – Pointer to a hal_wwdg_handle_t structure which contains the WWDG instance.
-
p_user_data – Pointer to the user data.
-
-
const
void
*
HAL_WWDG_GetUserData
(
const
hal_wwdg_handle_t
*
hwwdg
)
-
Retrieve User Data pointer from the handle.
- Parameters :
-
hwwdg – Pointer to a hal_wwdg_handle_t structure which contains the WWDG instance.
- Return values :
-
Pointer – to the user data.
-