LL CRC Functions ¶
CRC Configuration functions ¶
- group CRC_LL_EF_Configuration
-
Functions
-
void
LL_CRC_ResetCRCCalculationUnit
(
CRC_TypeDef
*
crcx
)
¶
-
Reset the CRC calculation unit.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR RESET LL_CRC_ResetCRCCalculationUnit
Note
If Programmable Initial CRC value feature is available, also set the Data Register to the value stored in the CRC_INIT register, otherwise, reset Data Register to its default value.
- Parameters :
-
crcx – CRC Instance
-
void
LL_CRC_SetPolynomialSize
(
CRC_TypeDef
*
crcx
,
uint32_t
poly_size
)
¶
-
Configure size of the polynomial.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR POLYSIZE LL_CRC_SetPolynomialSize
- Parameters :
-
-
crcx – CRC Instance
-
poly_size – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetPolynomialSize
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return size of the polynomial.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR POLYSIZE LL_CRC_GetPolynomialSize
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
input_reverse_mode
,
uint32_t
output_reverse_mode
)
¶
-
Configure the reversal of the bit order of the input and Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_X LL_CRC_SetDataReverseMode
Note
REV_X bit value of REV_IN and REV_OUT
- Parameters :
-
-
crcx – CRC Instance
-
input_reverse_mode – This parameter can be one of the following values:
-
output_reverse_mode – This parameter can be one of the following values:
-
-
void
LL_CRC_SetInputDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
input_reverse_mode
)
¶
-
Configure the reversal of the bit order of the input data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_IN LL_CRC_SetInputDataReverseMode
- Parameters :
-
-
crcx – CRC Instance
-
input_reverse_mode – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetInputDataReverseMode
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return type of reversal for input data bit order.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_IN LL_CRC_GetInputDataReverseMode
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetOutputDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
output_reverse_mode
)
¶
-
Configure the reversal of the bit order of the Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_OUT LL_CRC_SetOutputDataReverseMode
- Parameters :
-
-
crcx – CRC Instance
-
output_reverse_mode – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetOutputDataReverseMode
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return type of reversal of the bit order of the Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_OUT LL_CRC_GetOutputDataReverseMode
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetInitialData
(
CRC_TypeDef
*
crcx
,
uint32_t
crc_init_value
)
¶
-
Initialize the Programmable initial CRC value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
INIT INIT LL_CRC_SetInitialData
Note
If the CRC size is less than 32 bits, the least significant bits are used to write the correct value
Note
LL_CRC_DEFAULT_CRC_INITVALUE could be used as value for InitCrc parameter.
- Parameters :
-
-
crcx – CRC Instance
-
crc_init_value – Value to be programmed in Programmable initial CRC value register
-
-
uint32_t
LL_CRC_GetInitialData
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return current Initial CRC value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
INIT INIT LL_CRC_GetInitialData
Note
If the CRC size is less than 32 bits, the least significant bits are used to read the correct value
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – programmed in Programmable initial CRC value register
-
void
LL_CRC_SetPolynomialCoef
(
CRC_TypeDef
*
crcx
,
uint32_t
polynomial_coefficient
)
¶
-
Initialize the Programmable polynomial value (coefficients of the polynomial to be used for CRC calculation).
- Reference Manual to LL API cross reference (Register Field Functions)
-
POL POL LL_CRC_SetPolynomialCoef
Note
LL_CRC_DEFAULT_CRC32_POLY could be used as value for PolynomCoef parameter.
Note
Please check Reference Manual and existing Errata Sheets, regarding possible limitations for Polynomial values usage. For example, for a polynomial of degree 7, X^7 + X^6 + X^5 + X^2 + 1 is written 0x65
- Parameters :
-
-
crcx – CRC Instance
-
polynomial_coefficient – Value to be programmed in Programmable Polynomial value register
-
-
uint32_t
LL_CRC_GetPolynomialCoef
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return current Programmable polynomial value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
POL POL LL_CRC_GetPolynomialCoef
Note
Please check Reference Manual and existing Errata Sheets, regarding possible limitations for Polynomial values usage. For example, for a polynomial of degree 7, X^7 + X^6 + X^5 + X^2 + 1 is written 0x65
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – programmed in Programmable Polynomial value register
-
void
LL_CRC_ResetCRCCalculationUnit
(
CRC_TypeDef
*
crcx
)
¶
- group CRC_LL_EF_Configuration
-
Functions
-
void
LL_CRC_ResetCRCCalculationUnit
(
CRC_TypeDef
*
crcx
)
-
Reset the CRC calculation unit.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR RESET LL_CRC_ResetCRCCalculationUnit
Note
If Programmable Initial CRC value feature is available, also set the Data Register to the value stored in the CRC_INIT register, otherwise, reset Data Register to its default value.
- Parameters :
-
crcx – CRC Instance
-
void
LL_CRC_SetPolynomialSize
(
CRC_TypeDef
*
crcx
,
uint32_t
poly_size
)
-
Configure size of the polynomial.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR POLYSIZE LL_CRC_SetPolynomialSize
- Parameters :
-
-
crcx – CRC Instance
-
poly_size – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetPolynomialSize
(
const
CRC_TypeDef
*
crcx
)
-
Return size of the polynomial.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR POLYSIZE LL_CRC_GetPolynomialSize
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
input_reverse_mode
,
uint32_t
output_reverse_mode
)
-
Configure the reversal of the bit order of the input and Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_X LL_CRC_SetDataReverseMode
Note
REV_X bit value of REV_IN and REV_OUT
- Parameters :
-
-
crcx – CRC Instance
-
input_reverse_mode – This parameter can be one of the following values:
-
output_reverse_mode – This parameter can be one of the following values:
-
-
void
LL_CRC_SetInputDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
input_reverse_mode
)
-
Configure the reversal of the bit order of the input data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_IN LL_CRC_SetInputDataReverseMode
- Parameters :
-
-
crcx – CRC Instance
-
input_reverse_mode – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetInputDataReverseMode
(
const
CRC_TypeDef
*
crcx
)
-
Return type of reversal for input data bit order.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_IN LL_CRC_GetInputDataReverseMode
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetOutputDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
output_reverse_mode
)
-
Configure the reversal of the bit order of the Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_OUT LL_CRC_SetOutputDataReverseMode
- Parameters :
-
-
crcx – CRC Instance
-
output_reverse_mode – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetOutputDataReverseMode
(
const
CRC_TypeDef
*
crcx
)
-
Return type of reversal of the bit order of the Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_OUT LL_CRC_GetOutputDataReverseMode
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetInitialData
(
CRC_TypeDef
*
crcx
,
uint32_t
crc_init_value
)
-
Initialize the Programmable initial CRC value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
INIT INIT LL_CRC_SetInitialData
Note
If the CRC size is less than 32 bits, the least significant bits are used to write the correct value
Note
LL_CRC_DEFAULT_CRC_INITVALUE could be used as value for InitCrc parameter.
- Parameters :
-
-
crcx – CRC Instance
-
crc_init_value – Value to be programmed in Programmable initial CRC value register
-
-
uint32_t
LL_CRC_GetInitialData
(
const
CRC_TypeDef
*
crcx
)
-
Return current Initial CRC value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
INIT INIT LL_CRC_GetInitialData
Note
If the CRC size is less than 32 bits, the least significant bits are used to read the correct value
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – programmed in Programmable initial CRC value register
-
void
LL_CRC_SetPolynomialCoef
(
CRC_TypeDef
*
crcx
,
uint32_t
polynomial_coefficient
)
-
Initialize the Programmable polynomial value (coefficients of the polynomial to be used for CRC calculation).
- Reference Manual to LL API cross reference (Register Field Functions)
-
POL POL LL_CRC_SetPolynomialCoef
Note
LL_CRC_DEFAULT_CRC32_POLY could be used as value for PolynomCoef parameter.
Note
Please check Reference Manual and existing Errata Sheets, regarding possible limitations for Polynomial values usage. For example, for a polynomial of degree 7, X^7 + X^6 + X^5 + X^2 + 1 is written 0x65
- Parameters :
-
-
crcx – CRC Instance
-
polynomial_coefficient – Value to be programmed in Programmable Polynomial value register
-
-
uint32_t
LL_CRC_GetPolynomialCoef
(
const
CRC_TypeDef
*
crcx
)
-
Return current Programmable polynomial value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
POL POL LL_CRC_GetPolynomialCoef
Note
Please check Reference Manual and existing Errata Sheets, regarding possible limitations for Polynomial values usage. For example, for a polynomial of degree 7, X^7 + X^6 + X^5 + X^2 + 1 is written 0x65
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – programmed in Programmable Polynomial value register
-
void
LL_CRC_ResetCRCCalculationUnit
(
CRC_TypeDef
*
crcx
)
- group CRC_LL_EF_Configuration
-
Functions
-
void
LL_CRC_ResetCRCCalculationUnit
(
CRC_TypeDef
*
crcx
)
-
Reset the CRC calculation unit.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR RESET LL_CRC_ResetCRCCalculationUnit
Note
If Programmable Initial CRC value feature is available, also set the Data Register to the value stored in the CRC_INIT register, otherwise, reset Data Register to its default value.
- Parameters :
-
crcx – CRC Instance
-
void
LL_CRC_SetPolynomialSize
(
CRC_TypeDef
*
crcx
,
uint32_t
poly_size
)
-
Configure size of the polynomial.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR POLYSIZE LL_CRC_SetPolynomialSize
- Parameters :
-
-
crcx – CRC Instance
-
poly_size – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetPolynomialSize
(
const
CRC_TypeDef
*
crcx
)
-
Return size of the polynomial.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR POLYSIZE LL_CRC_GetPolynomialSize
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
input_reverse_mode
,
uint32_t
output_reverse_mode
)
-
Configure the reversal of the bit order of the input and Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_X LL_CRC_SetDataReverseMode
Note
REV_X bit value of REV_IN and REV_OUT
- Parameters :
-
-
crcx – CRC Instance
-
input_reverse_mode – This parameter can be one of the following values:
-
output_reverse_mode – This parameter can be one of the following values:
-
-
void
LL_CRC_SetInputDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
input_reverse_mode
)
-
Configure the reversal of the bit order of the input data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_IN LL_CRC_SetInputDataReverseMode
- Parameters :
-
-
crcx – CRC Instance
-
input_reverse_mode – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetInputDataReverseMode
(
const
CRC_TypeDef
*
crcx
)
-
Return type of reversal for input data bit order.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_IN LL_CRC_GetInputDataReverseMode
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetOutputDataReverseMode
(
CRC_TypeDef
*
crcx
,
uint32_t
output_reverse_mode
)
-
Configure the reversal of the bit order of the Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_OUT LL_CRC_SetOutputDataReverseMode
- Parameters :
-
-
crcx – CRC Instance
-
output_reverse_mode – This parameter can be one of the following values:
-
-
uint32_t
LL_CRC_GetOutputDataReverseMode
(
const
CRC_TypeDef
*
crcx
)
-
Return type of reversal of the bit order of the Output data.
- Reference Manual to LL API cross reference (Register Field Functions)
-
CR REV_OUT LL_CRC_GetOutputDataReverseMode
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Returned – value can be one of the following values:
-
void
LL_CRC_SetInitialData
(
CRC_TypeDef
*
crcx
,
uint32_t
crc_init_value
)
-
Initialize the Programmable initial CRC value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
INIT INIT LL_CRC_SetInitialData
Note
If the CRC size is less than 32 bits, the least significant bits are used to write the correct value
Note
LL_CRC_DEFAULT_CRC_INITVALUE could be used as value for InitCrc parameter.
- Parameters :
-
-
crcx – CRC Instance
-
crc_init_value – Value to be programmed in Programmable initial CRC value register
-
-
uint32_t
LL_CRC_GetInitialData
(
const
CRC_TypeDef
*
crcx
)
-
Return current Initial CRC value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
INIT INIT LL_CRC_GetInitialData
Note
If the CRC size is less than 32 bits, the least significant bits are used to read the correct value
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – programmed in Programmable initial CRC value register
-
void
LL_CRC_SetPolynomialCoef
(
CRC_TypeDef
*
crcx
,
uint32_t
polynomial_coefficient
)
-
Initialize the Programmable polynomial value (coefficients of the polynomial to be used for CRC calculation).
- Reference Manual to LL API cross reference (Register Field Functions)
-
POL POL LL_CRC_SetPolynomialCoef
Note
LL_CRC_DEFAULT_CRC32_POLY could be used as value for PolynomCoef parameter.
Note
Please check Reference Manual and existing Errata Sheets, regarding possible limitations for Polynomial values usage. For example, for a polynomial of degree 7, X^7 + X^6 + X^5 + X^2 + 1 is written 0x65
- Parameters :
-
-
crcx – CRC Instance
-
polynomial_coefficient – Value to be programmed in Programmable Polynomial value register
-
-
uint32_t
LL_CRC_GetPolynomialCoef
(
const
CRC_TypeDef
*
crcx
)
-
Return current Programmable polynomial value.
- Reference Manual to LL API cross reference (Register Field Functions)
-
POL POL LL_CRC_GetPolynomialCoef
Note
Please check Reference Manual and existing Errata Sheets, regarding possible limitations for Polynomial values usage. For example, for a polynomial of degree 7, X^7 + X^6 + X^5 + X^2 + 1 is written 0x65
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – programmed in Programmable Polynomial value register
-
void
LL_CRC_ResetCRCCalculationUnit
(
CRC_TypeDef
*
crcx
)
Data_Management ¶
- group CRC_LL_EF_Data_Management
-
Functions
-
void
LL_CRC_FeedData32
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
¶
-
Write given 32-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData32
- Parameters :
-
-
crcx – CRC Instance
-
in_data – value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFFFFFFFF
-
-
void
LL_CRC_FeedData16
(
CRC_TypeDef
*
crcx
,
uint16_t
in_data
)
¶
-
Write given 16-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData16
- Parameters :
-
-
crcx – CRC Instance
-
in_data – 16 bit value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFFFF
-
-
void
LL_CRC_FeedData8
(
CRC_TypeDef
*
crcx
,
uint8_t
in_data
)
¶
-
Write given 8-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData8
- Parameters :
-
-
crcx – CRC Instance
-
in_data – 8 bit value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFF
-
-
uint32_t
LL_CRC_ReadData32
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return current CRC calculation result. 32 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData32
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (32 bits).
-
uint16_t
LL_CRC_ReadData16
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return current CRC calculation result. 16 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData16
Note
This function is expected to be used in a 16 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (16 bits).
-
uint8_t
LL_CRC_ReadData8
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return current CRC calculation result. 8 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData8
Note
This function is expected to be used in a 8 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (8 bits).
-
uint8_t
LL_CRC_ReadData7
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return current CRC calculation result. 7 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData7
Note
This function is expected to be used in a 7 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (7 bits).
-
uint32_t
LL_CRC_ReadIDR
(
const
CRC_TypeDef
*
crcx
)
¶
-
Return data stored in the Independent Data(IDR) register.
- Reference Manual to LL API cross reference (Register Field Functions)
-
IDR IDR LL_CRC_ReadIDR
Note
This register can be used as a temporary storage location for one 32-bit long data.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – stored in CRC_IDR register (General-purpose 32-bit data register).
-
void
LL_CRC_WriteIDR
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
¶
-
Store data in the Independent Data(IDR) register.
- Reference Manual to LL API cross reference (Register Field Functions)
-
IDR IDR LL_CRC_WriteIDR
Note
This register can be used as a temporary storage location for one 32-bit long data.
- Parameters :
-
-
crcx – CRC Instance
-
in_data – value to be stored in CRC_IDR register (32-bit) between Min_Data=0 and Max_Data=0xFFFFFFFF
-
-
void
LL_CRC_FeedData32
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
¶
- group CRC_LL_EF_Data_Management
-
Functions
-
void
LL_CRC_FeedData32
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
-
Write given 32-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData32
- Parameters :
-
-
crcx – CRC Instance
-
in_data – value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFFFFFFFF
-
-
void
LL_CRC_FeedData16
(
CRC_TypeDef
*
crcx
,
uint16_t
in_data
)
-
Write given 16-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData16
- Parameters :
-
-
crcx – CRC Instance
-
in_data – 16 bit value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFFFF
-
-
void
LL_CRC_FeedData8
(
CRC_TypeDef
*
crcx
,
uint8_t
in_data
)
-
Write given 8-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData8
- Parameters :
-
-
crcx – CRC Instance
-
in_data – 8 bit value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFF
-
-
uint32_t
LL_CRC_ReadData32
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 32 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData32
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (32 bits).
-
uint16_t
LL_CRC_ReadData16
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 16 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData16
Note
This function is expected to be used in a 16 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (16 bits).
-
uint8_t
LL_CRC_ReadData8
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 8 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData8
Note
This function is expected to be used in a 8 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (8 bits).
-
uint8_t
LL_CRC_ReadData7
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 7 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData7
Note
This function is expected to be used in a 7 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (7 bits).
-
uint32_t
LL_CRC_ReadIDR
(
const
CRC_TypeDef
*
crcx
)
-
Return data stored in the Independent Data(IDR) register.
- Reference Manual to LL API cross reference (Register Field Functions)
-
IDR IDR LL_CRC_ReadIDR
Note
This register can be used as a temporary storage location for one 32-bit long data.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – stored in CRC_IDR register (General-purpose 32-bit data register).
-
void
LL_CRC_WriteIDR
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
-
Store data in the Independent Data(IDR) register.
- Reference Manual to LL API cross reference (Register Field Functions)
-
IDR IDR LL_CRC_WriteIDR
Note
This register can be used as a temporary storage location for one 32-bit long data.
- Parameters :
-
-
crcx – CRC Instance
-
in_data – value to be stored in CRC_IDR register (32-bit) between Min_Data=0 and Max_Data=0xFFFFFFFF
-
-
void
LL_CRC_FeedData32
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
- group CRC_LL_EF_Data_Management
-
Functions
-
void
LL_CRC_FeedData32
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
-
Write given 32-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData32
- Parameters :
-
-
crcx – CRC Instance
-
in_data – value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFFFFFFFF
-
-
void
LL_CRC_FeedData16
(
CRC_TypeDef
*
crcx
,
uint16_t
in_data
)
-
Write given 16-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData16
- Parameters :
-
-
crcx – CRC Instance
-
in_data – 16 bit value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFFFF
-
-
void
LL_CRC_FeedData8
(
CRC_TypeDef
*
crcx
,
uint8_t
in_data
)
-
Write given 8-bit data to the CRC calculator.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_FeedData8
- Parameters :
-
-
crcx – CRC Instance
-
in_data – 8 bit value to be provided to CRC calculator between Min_Data=0 and Max_Data=0xFF
-
-
uint32_t
LL_CRC_ReadData32
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 32 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData32
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (32 bits).
-
uint16_t
LL_CRC_ReadData16
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 16 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData16
Note
This function is expected to be used in a 16 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (16 bits).
-
uint8_t
LL_CRC_ReadData8
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 8 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData8
Note
This function is expected to be used in a 8 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (8 bits).
-
uint8_t
LL_CRC_ReadData7
(
const
CRC_TypeDef
*
crcx
)
-
Return current CRC calculation result. 7 bits value is returned.
- Reference Manual to LL API cross reference (Register Field Functions)
-
DR DR LL_CRC_ReadData7
Note
This function is expected to be used in a 7 bits CRC polynomial size context.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Current – CRC calculation result as stored in CRC_DR register (7 bits).
-
uint32_t
LL_CRC_ReadIDR
(
const
CRC_TypeDef
*
crcx
)
-
Return data stored in the Independent Data(IDR) register.
- Reference Manual to LL API cross reference (Register Field Functions)
-
IDR IDR LL_CRC_ReadIDR
Note
This register can be used as a temporary storage location for one 32-bit long data.
- Parameters :
-
crcx – CRC Instance
- Return values :
-
Value – stored in CRC_IDR register (General-purpose 32-bit data register).
-
void
LL_CRC_WriteIDR
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)
-
Store data in the Independent Data(IDR) register.
- Reference Manual to LL API cross reference (Register Field Functions)
-
IDR IDR LL_CRC_WriteIDR
Note
This register can be used as a temporary storage location for one 32-bit long data.
- Parameters :
-
-
crcx – CRC Instance
-
in_data – value to be stored in CRC_IDR register (32-bit) between Min_Data=0 and Max_Data=0xFFFFFFFF
-
-
void
LL_CRC_FeedData32
(
CRC_TypeDef
*
crcx
,
uint32_t
in_data
)