Interface TIME Functions ¶
TIME HAL Tick Interface Functions ¶
-
ee_itf_time_status
EE_ITF_TIME_Init
(
void
*
time_object
)
¶
-
Initialize the time interface context.
- Parameters :
-
time_object – Time base instance used by the interface (unused with the HAL tick time base).
- Return values :
-
Possible – return values: see ee_itf_time_status.
-
uint32_t
EE_ITF_TIME_Get
(
void
)
¶
-
Return the current time base value, in milliseconds.
- Return values :
-
uint32_t – free-running millisecond counter provided by HAL_GetTick().
TIME Template Interface Functions ¶
-
ee_itf_time_status
EE_ITF_TIME_Init
(
void
*
time_object
)
-
Initialize the time interface context (template).
Initialize the time interface context.
- Parameters :
-
time_object – Time base instance used by the interface.
- Return values :
-
Possible – return values: see ee_itf_time_status.
-
uint32_t
EE_ITF_TIME_Get
(
void
)
-
Return the current time base value, in milliseconds (template).
Return the current time base value, in milliseconds.
- Return values :
-
uint32_t – free-running millisecond counter.