FreeRTOS Examples list

Example name

Description

mutex

The example demonstrates how to configure and use the FreeRTOS™ API to synchronize two threads using a mutex.

message_queue

The example demonstrates how to configure and use the FreeRTOS API to synchronize between threads using message queue.

low_power

Configure the LowPower based on TICKLESS_IDLE feature. Make system enter stop mode and wakeup on LPTIM interrupt.

task_notification

The example demonstrates how to configure and use the FreeRTOS API to synchronize between threads using task notification and software timers.

See FreeRTOS examples