HTS221 Part Drivers API Documentation - Core ¶
This page documents the API of the Core component of the HTS221 Part Drivers.
An overview of the driver is also available here: main_doc .
Functions ¶
Functions
-
hts221_drv_status_t
hts221_drv_init
(
hts221_object_t
*
p_obj
,
uint32_t
id
)
¶
-
initialize the HTS221 sensor.
- Parameters :
-
p_obj – the device object
id – the device instance id
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_deinit
(
hts221_object_t
*
p_obj
)
¶
-
deinitialize the HTS221 sensor.
- Parameters :
-
p_obj – the device object
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_read_id
(
hts221_object_t
*
p_obj
,
uint8_t
*
id
)
¶
-
get who_am_i value.
- Parameters :
-
p_obj – the device object
id – the who_am_i value
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_get_init_status
(
hts221_object_t
*
p_obj
,
uint8_t
*
status
)
¶
-
get the hts221 initialization status.
- Parameters :
-
p_obj – the device object
status – 1 if initialized, 0 otherwise
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_enable
(
hts221_object_t
*
p_obj
)
¶
-
enable the hts221 sensor.
- Parameters :
-
p_obj – the device object
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_disable
(
hts221_object_t
*
p_obj
)
¶
-
disable the hts221 humidity sensor.
- Parameters :
-
p_obj – the device object
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_get_outputdatarate
(
hts221_object_t
*
p_obj
,
float_t
*
odr
)
¶
-
get output data rate.
- Parameters :
-
p_obj – the device object
odr – the output data rate value
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_set_outputdatarate
(
hts221_object_t
*
p_obj
,
float_t
odr
)
¶
-
set output data rate.
- Parameters :
-
p_obj – the device p_obj
odr – the output data rate value to be set
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_get_humidity
(
hts221_object_t
*
p_obj
,
float_t
*
value
)
¶
-
get the HTS221 humidity value.
- Parameters :
-
p_obj – the device object
value – pointer where the humidity value is written
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_hum_get_drdy_status
(
hts221_object_t
*
p_obj
,
uint8_t
*
status
)
¶
-
get the HTS221 humidity data-ready bit value.
- Parameters :
-
p_obj – the device p_obj
status – the status of the data-ready bit
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_get_temperature
(
hts221_object_t
*
p_obj
,
float_t
*
value
)
¶
-
get the HTS221 temperature value.
- Parameters :
-
p_obj – the device p_obj
value – pointer where the temperature value is written
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_temp_get_drdy_status
(
hts221_object_t
*
p_obj
,
uint8_t
*
status
)
¶
-
get the hts221 temperature data-ready bit value.
- Parameters :
-
p_obj – the device p_obj
status – the status of the data-ready bit
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_read_reg
(
hts221_object_t
*
p_obj
,
uint8_t
reg
,
uint8_t
*
data
)
¶
-
get the hts221 register value.
- Parameters :
-
p_obj – the device object
reg – address to be read
data – pointer where the value is written
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_write_reg
(
hts221_object_t
*
p_obj
,
uint8_t
reg
,
uint8_t
data
)
¶
-
set the hts221 register value.
- Parameters :
-
p_obj – the device object
reg – address to be written
data – value to be written
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_set_one_shot
(
hts221_object_t
*
p_obj
)
¶
-
set the hts221 one-shot mode.
- Parameters :
-
p_obj – the device p_obj
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_get_one_shot_status
(
hts221_object_t
*
p_obj
,
uint8_t
*
status
)
¶
-
get the hts221 one shot status.
- Parameters :
-
p_obj – the device p_obj
status – pointer to the one shot status
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_enable_drdy_interrupt
(
hts221_object_t
*
p_obj
)
¶
-
enable hts221 drdy interrupt mode.
- Parameters :
-
p_obj – the device object
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_enable_irq
(
hts221_object_t
*
p_obj
)
¶
-
Enable the interrupt.
- Parameters :
-
p_obj – the device instance object
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_disable_irq
(
hts221_object_t
*
p_obj
)
¶
-
disable the interrupt.
- Parameters :
-
p_obj – the device instance object
- Return values :
-
0 – in case of success, an error code otherwise
-
hts221_drv_status_t
hts221_drv_register_callback
(
hts221_object_t
*
pobj
,
hts221_callback_t
cb
,
void
*
arg
)
¶
-
Register the callback function for interrupt events.
- Parameters :
-
p_obj – the device instance object
cb – the callback function
arg – the optional argument given to the callback
- Return values :
-
0 – in case of success, an error code otherwise
Types ¶
Enums
Typedefs
-
typedef
struct
hts221_object_s
hts221_object_t
¶
-
HTS221 object structure type callback function pointer definition
-
typedef
void
(
*
hts221_callback_t
)
(
hts221_object_t
*
pobj
,
void
*
arg
)
¶
-
struct
hts221_object_s
¶
-
HTS221 object structure.
-
struct
hts221_cb_ctx_t
¶
-
Callback context structure.
Public Members
-
hts221_callback_t
callback
¶
-
Callback function to register
-
void
*
arg
¶
-
Optional argument given to the callback
-
hts221_callback_t
callback
¶
-
struct
lin_t
¶
-
HTS221 output value linearized structure.
-
union
hts221_axis3bit16_t
¶
-
#include <hts221.h>
HTS221 3 axis 16 bit union.
-
union
hts221_axis1bit16_t
¶
-
#include <hts221.h>
HTS221 1 axis 16 bit union.
-
union
hts221_axis3bit32_t
¶
-
#include <hts221.h>
HTS221 3 axis 32 bit union.
-
union
hts221_axis1bit32_t
¶
-
#include <hts221.h>
HTS221 1 axis 32 bit union.
Constants and macros ¶
Defines
-
HTS221_I2C_BUS
0U
¶
-
HTS221_I2C_BUS
-
HTS221_SPI_3WIRES_BUS
1U
¶
-
HTS221_SPI_3WIRES_BUS
-
HTS221_ODR_0_HZ_FP
0.0f
¶
-
0 Hz output data rate
-
HTS221_ODR_1_HZ_FP
1.0f
¶
-
1 Hz output data rate
-
HTS221_ODR_7_HZ_FP
7.0f
¶
-
7 Hz output data rate
-
HTS221_ODR_12_HZ_5_FP
12.5f
¶
-
12.5 Hz output data rate
-
HTS221_MAX_ODR
12.5f
¶
-
temperature maximum output data rate
-
HTS221_MAX_HUM_VALUE
100.0f
¶
-
humidity maximum value
-
HTS221_MIN_HUM_VALUE
0.0f
¶
-
humidity minimum value