Device Startup Files ¶
For STM32C5 series the CMSIS Device Startup files are provided in the DFP pack
Source/startup_stm32c5nnxx.h : device startup file
Note
Starting from CMSIS-Core 5.6.0 , Arm switched from assembly to C language for the CMSIS Device Startup files, to provide:
Improved readability : easier to understand and modify.
Better maintainability : easier to debug and extend, no more assembly language expertise required.
Enhanced portability : easier to adapt to different toolchains and architectures.
The startup file defines device exceptions and interrupts, and provides their initial (weak) handler functions.
Specifically, following functionalities are provided:
The reset handler
Reset_Handlerwhich is executed upon CPU reset and typically calls theSystemInit()function. After the system init the control is transferred to the C/C++ run-time library which performs initialization and calls the main function in the user code.The setup values for the Main Stack Pointer (MSP).
Exception vectors of the Cortex-M Processor with weak functions that implement default routines.
Interrupt vectors that are device specific with weak functions that implement default routines.
Default_IRQHandler_Hookfunction that can be implemented by the user to customize the default behavior of all unimplemented interrupts in a single place at application level.