HAL JPEG Overview ¶
Introducing JPEG ¶
- group JPEG_Introduction
-
-
This introduction is under development.
-
Module and files ¶
The following diagram illustrates the JPEG module and its associated files.
Component diagram ¶
The following diagram illustrates the software components involved in the JPEG module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.
Configuration table ¶
The following table lists the configuration defines for the HAL JPEG module, specifying their locations, default values, and descriptions:
- group JPEG_Configuration_Table
-
¶
Configuration inside the JPEG driver ¶
Config defines
Description
Default value
Note
PRODUCT
from IDE
None
The selected device.
USE_HAL_JPEG_MODULE
from hal_conf.h
1U
Allows to use HAL JPEG module.
USE_ASSERT_DBG_PARAM
from IDE
None
Allows to use the assert check parameters.
USE_ASSERT_DBG_STATE
from IDE
None
Allows to use the assert check states.
USE_HAL_CHECK_PARAM
from hal_conf.h
0
Allows to use the run-time checks parameters.
USE_HAL_JPEG_DMA
from hal_conf.h
0
Allows to use DMA mode.
USE_HAL_JPEG_REGISTER_CALLBACKS
from hal_conf.h
0
Allows to use register callbacks.
USE_HAL_JPEG_CLK_ENABLE_MODEL
from hal_conf.h
HAL_CLK_ENABLE_NO
Allows to use the clock enable model.
USE_HAL_JPEG_GET_LAST_ERRORS
from hal_conf.h
0
Allows to use error code mechanism.