HAL MDF Overview ¶
Introducing MDF ¶
- group MDF_Introduction
-
-
This introduction is under development.
-
Module and files ¶
The following diagram illustrates the MDF module and its associated files.
Component diagram ¶
The following diagram illustrates the software components involved in the MDF module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.
Configuration table ¶
The following table lists the configuration defines for the HAL MDF module, specifying their locations, default values, and descriptions:
- group MDF_Configuration_Table
-
Configuration inside the HAL MDF driver ¶
Config defines
Where
Default value
Note
USE_HAL_MDF_MODULE
hal_conf.h
1
Enable the HAL MDF module
USE_HAL_MDF_REGISTER_CALLBACKS
hal_conf.h
0
Allow user to define his own callback
USE_HAL_MDF_CLK_ENABLE_MODEL
hal_conf.h
HAL_CLK_ENABLE_NO
Enable the gating of the peripheral clock
USE_HAL_MDF_USER_DATA
hal_conf.h
0
Add an user data inside HAL MDF handle
USE_HAL_MDF_GET_LAST_ERRORS
hal_conf.h
0
Enable retrieving last processes error codes
USE_HAL_MDF_DMA
hal_conf.h
1
Enable DMA code inside HAL MDF
USE_HAL_CHECK_PARAM
hal_conf.h
0
Enable checking of vital parameters at runtime
USE_HAL_CHECK_PROCESS_STATE
hal_conf.h
0
Enable atomic access to process state check
USE_ASSERT_DBG_PARAM
PreProcessor env
NONE
Enable check parameters for HAL
USE_ASSERT_DBG_STATE
PreProcessor env
NONE
Enable check state for HAL