HAL NOR Overview ¶
Introducing NOR ¶
- group NOR_Introduction
-
-
This introduction is under development.
-
Module and files ¶
The following diagram illustrates the NOR module and its associated files.
Component diagram ¶
The following diagram illustrates the software components involved in the NOR module. It shows the interactions between the user application, HAL drivers, low-level drivers, and the hardware components.
Configuration table ¶
The following table lists the configuration defines for the HAL NOR module, specifying their locations, default values, and descriptions:
- group NOR_Configuration_Table
-
¶
Configuration inside the NOR driver ¶
Config defines
Description
Default value
Note
USE_ASSERT_DBG_PARAM
from IDE
NA
Allows to use the assert check parameters.
USE_ASSERT_DBG_STATE
from IDE
NA
Allows to use the assert check states.
USE_HAL_CHECK_PARAM
from hal_conf.h
0U
Allows to use the run-time check parameters.
USE_HAL_CHECK_PROCESS_STATE
from hal_conf.h
0U
Allows to ensure a safe state transition.
USE_HAL_NOR_MODULE
from hal_conf.h
1U
Allows to use the HAL NOR module.
USE_HAL_NOR_PROTECTION
from hal_conf.h
0U
Allows to enable program protection register.
USE_FMC_CLK_ENABLE_MODEL
from hal_conf.h
HAL_CLK_ENABLE_NO
Allows to enable the FMC clock.
USE_HAL_NOR_USER_DATA
from hal_conf.h
0U
Allows to use user data.