Install STM32Cube for Agentic AI¶
The STM32Cube for Agentic AI Toolkit (beta) provides STM32Cube Agentic Contexts to
AI coding agents. Use cube agentic-ai setup for the typical route: it
installs all contexts compatible with the selected target and deploys them
into a project folder. The setup command supports six editor-and-agent
combinations: see
Target, prerequisites, and project folder.
Important
This STM32Cube for Agentic AI Toolkit does not itself perform AI inference or make autonomous decisions
Installation methods¶
Paste one prompt into an AI coding agent. It confirms the license,
target, project folder, profile, and consent before running setup.
Install the CLI and installer, then run setup. Preview and update steps are optional.
Before either path, review Target, prerequisites, and project folder for supported targets, prerequisites, and project/workspace folder guidance. See Choose your installation for a decision diagram covering typical and custom installations, Python, and VS Code profiles.
Each method offers a typical installation with all compatible contexts and a custom installation with interactive context and service selection. Both support target selection. To update an existing installation, see Updates.
For host requirements, beta limitations, and the current context inventory, see the STM32Cube for Agentic AI documentation. For command details, see the installer user manual.
Licenses¶
STM32CubeCLI is distributed under the SLA0048 software license agreement. The STM32Cube for Agentic AI bundles are distributed under the SLA0044 software license agreement. Tool dependencies, such as the STM32CubeMX2 application and STM32CubeProgrammer, have their own license agreements. Installing a bundle means accepting its license agreement.
cube bundle install asks for license acceptance. setup installs the
contexts and their tool dependencies without license prompts: running it, or
sending the agent prompt, is the acceptance, and its result lists the licenses
in data.licenses. To read a license before installation, run:
cube bundle license --online cube-agentic-ai-installer
To see what setup would install without installing it, run
cube agentic-ai setup --dry-run.
Contexts of this release¶
The installer catalog defines the contexts available to the installation. The catalog can change independently of this page. See the current context inventory and versions for the latest list. The installer is the central point for catalog and context updates.
Note
This toolkit is a beta and receives regular context and guidance updates. Review the current limitations in the user documentation.