Supported contexts and versions

The table lists reference bundle versions for this release, checked on November 2, 2026. The toolkit does not have one shared bundle version. Contexts are updated independently, and the installer catalog can change when new contexts or routing guidance are released. Use the commands below to check installed versions rather than assuming this table matches every machine.

Context

Scope

Bundle

Reference version

STM32Cube for Agentic AI installer

Installs context bundles on the machine and deploys selected context files into a project.

cube-agentic-ai-installer

1.0.0

STM32Cube Build

Checks prerequisites and builds CMake-based STM32 projects.

cube-agentic-ai-build

1.0.0

STM32CubeCLI

Guides STM32CubeCLI commands, bundles, dependencies, licenses, and downloads.

cube-agentic-ai-cube-wrapper

1.0.3

STM32 DAP Debug

Prepares and launches STM32 debug sessions through DebugMCP.

cube-agentic-ai-debug-dap

1.0.0

STM32 Errata Hunter

Finds and analyzes published silicon errata.

cube-agentic-ai-errata-hunter

1.0.0

STM32Cube Embedded Software

Discovers examples, provides HAL/LL guidance, and assists with application code.

cube-agentic-ai-esw

1.0.0

STM32CubeMX2

Creates, configures, and generates STM32CubeMX2 projects.

cube-agentic-ai-mx2-skill

1.0.0

STM32CubeProgrammer

Programs internal and external NVM, erases and reads memory, and programs option bytes on STM32 MCUs. STM32 MPUs are not covered.

cube-agentic-ai-programmer

1.0.0

STM32 Sidekick Knowledge Base

Searches supported STM32 knowledge-base sources with provenance.

cube-agentic-ai-sidekick-kb

1.0.0

ST Official Documentation

Discovers official ST documents and retrieves available assets.

cube-agentic-ai-st-docs

1.0.0

The installer is separate from the technical contexts. Its release-reference version is 1.0.0. Update it when the catalog gains contexts or its general project guidance changes.

Check installed versions and supported contexts with:

cube agentic-ai machine-discovery --ai-only --no-json
cube agentic-ai show-catalog

For each context’s service identifiers and descriptions, use its discovery command, for example cube cube-agentic-ai-esw --list-ai-services. See STM32Cube Embedded Software Context for the eSW service mapping.

Update the installer first, then ask it to install or update eligible contexts from the configured registry:

cube bundle update cube-agentic-ai-installer
cube agentic-ai machine-bootstrap --upgrade-installed-in-range true

Updating a machine bundle does not change a deployed project. Before deploying a newer context version, remove the old context from the project, add the new version, then resolve its requirements. Run doctor <project-folder> and follow the target-preserving update commands in data.nextSteps:

cube agentic-ai doctor <project-folder> --fix

The registry can change after this page is built. Run machine-discovery for installed versions and show-catalog for the latest catalog carried by the installed installer.