Supported IDEs and AI coding agents¶
The installer deploys the Agentic Contexts to every supported AI coding agent.
It adapts only the folder names, the file formats and the MCP configuration
file to what each agent reads. The concepts, such as skills, agents,
instructions and MCP servers, are the same everywhere. Two contexts depend on
STM32CubeIDE for Visual Studio Code and are available only with
--ide vscode, as described in
Contexts that need VS Code.
You choose the target with two options of the cube agentic-ai commands:
--agentic-systemselects the AI coding agent:github-copilot,claude-codeorcursor. It decides where skills, agents, instructions, the routing skill and the MCP configuration file are written, because the agent is the MCP client that reads them.--ideselects the editor that hosts the agent:vscode,cursorornonefor a terminal session without an editor. It decides which editor extensions the installer proposes. It changes the MCP file only for GitHub Copilot in VS Code.
Supported combinations¶
Six combinations are supported. The installer rejects any other pair with the
error TARGET_COMBINATION_NOT_SUPPORTED, for example --ide cursor with
--agentic-system github-copilot. The option --canonical writes only the
portable .cube-ai/ layout and skips this check.
Here, supported means that the installer accepts the target and writes its documented configuration. It does not mean every agent and editor combination has been integration-tested. See Known limitations for the current validation coverage.
AI coding agent and editor |
Options |
MCP configuration file |
Skills, agents and instructions |
Project instruction file |
|---|---|---|---|---|
GitHub Copilot in VS Code |
|
|
|
|
GitHub Copilot CLI, no editor |
|
|
|
|
Claude Code CLI, no editor |
|
|
|
|
Claude Code extension in VS Code |
|
|
|
|
Cursor editor |
|
|
|
|
Cursor CLI, no editor |
|
|
|
|
The project instruction file is the file that the agent reads at the start of every session. The installer proposes the statement that routes STM32 requests to the routing skill, and you add it to that file.
For agent-specific VS Code extension prerequisites, see Prerequisites.
The installer deploys contexts into a project or workspace, not into the user home directory. Select contexts for each project independently. Only the context bundles are installed at machine scope. Project locks record the versions and services deployed in that project. See Supported contexts and versions for the current bundle versions.
The default target is GitHub Copilot in VS Code. To use another combination,
pass both options on the setup, project-add and project-deploy
commands. For example, for the Claude Code CLI:
cube agentic-ai project-add <bundle> <project> --ide none --agentic-system claude-code
Contexts that need VS Code¶
The STM32Cube Build Context and the
STM32 DAP Debug Context need
STM32CubeIDE for Visual Studio Code. The installer deploys them only when
--ide vscode is used, whatever the AI coding agent. With --ide none,
--ide cursor or --canonical, the installer does not install them.
setup lists them as unavailable, and a project-add or setup command
that names one of them fails with an error. All other contexts are available in
the six combinations.
Combination |
Build |
DAP Debug |
Other contexts |
|---|---|---|---|
GitHub Copilot in VS Code |
Yes |
Yes |
Yes |
Claude Code extension in VS Code |
Yes |
Yes |
Yes |
GitHub Copilot CLI, Claude Code CLI |
No |
No |
Yes |
Cursor editor, Cursor CLI |
No |
No |
Yes |
How each agent reads the deployed files¶
GitHub Copilot¶
Copilot in VS Code reads the MCP servers from
.vscode/mcp.json, under the keyservers. See the VS Code MCP servers documentation.Copilot CLI does not read
.vscode/mcp.json. It reads.mcp.jsonfrom the working directory up to the repository root, under the keymcpServers. It also reads.github/mcp.json, but only inside a Git repository, so the installer writes.mcp.json. See the Copilot CLI MCP documentation.Skills are read from
.github/skills/. See the GitHub documentation on agent skills.
Claude Code¶
The Claude Code CLI and the Claude Code extension in VS Code share the same configuration. Both read
.mcp.json, under the keymcpServers. See the Claude Code MCP documentation and the Claude Code VS Code documentation.Skills are read from
.claude/skills/. See the Claude Code skills documentation.Claude Code reads
CLAUDE.mdas the project instruction file. It readsAGENTS.mdonly when noCLAUDE.mdexists. See the Claude Code memory documentation.
Cursor¶
The Cursor editor and the Cursor CLI share the same project files. Both read
.cursor/mcp.json, under the keymcpServers. See the Cursor MCP documentation and the Cursor CLI MCP documentation.Skills are read from
.cursor/skills/<name>/SKILL.mdand subagents from.cursor/agents/. See the Cursor skills documentation and the Cursor subagents documentation.Cursor loads rules only from
.cursor/rules/*.mdc. The installer converts each instruction to a rule: an instruction that applies to every file becomes an always-on rule, and an instruction with a file pattern becomes a rule that Cursor attaches when matching files are in the context. See the Cursor rules documentation.
Approve the MCP servers before first use¶
Each agent asks you to approve project MCP servers before it starts them. The installer cannot do this step for you.
Combination |
What to do |
|---|---|
GitHub Copilot in VS Code |
Trust the workspace, then start the servers from |
GitHub Copilot CLI |
Start |
Claude Code CLI, Claude Code extension in VS Code |
Start |
Cursor editor, Cursor CLI |
Enable the servers in the Cursor settings, or run
|
Note
If you start Copilot CLI from the terminal of a VS Code window that has the
project folder open, Copilot CLI connects to that window and does not load
the project .mcp.json. Run Copilot CLI from a terminal outside VS Code,
or use Copilot Chat in VS Code.
One target per project¶
A project has one target. After you deploy a context, the installer rejects a
command that asks for another --ide, --agentic-system or
--canonical with the error TARGET_CHANGED_IN_DEPLOYED_PROJECT, and it
changes nothing. To move a project to another target, remove each deployed
context with project-remove, then deploy again with the new target.
Not supported¶
The installer does not provide native configuration for agents or editors
outside the six combinations above. For another agentic system,
--canonical writes the portable .cube-ai/ layout. You must adapt it
manually for that agent. This is not an additional native or integration-tested
target. A pairing outside the table is rejected unless --canonical is
used.
For the exact behavior of each option, see the installer user manual.