User interactions ¶
The STM32Cube Software Examples are designed to illustrate the use of the STM32 in various applicative use-cases. We do not provide ready-to-use product level applications, but a set of meaningful use-cases that can be used as a starting point for your own STM32 applications. The implementation is minimalist, yet functional, and is meant to be used as a way to learn how to use the STM32 peripherals and software.
A user action is a specific task that the user can perform to interact with the example. The examples are designed to offer the required user actions so that it is easy:
-
To trigger the required events (for example by pressing a button).
-
To view the outcome of the scenario (for example by observing the LEDs).
-
To follow the sequence of actions (for example by observing the serial output).
-
To follow the execution flow of the example code (for example by using a debugger).
-
To observe the signals on the pins of the STM32 (for example by using an oscilloscope).
Using the board parts ¶
As the STM32Cube Software Examples are designed to be used on various STM32 boards, the user actions are implemented using the minimal set of board parts:
-
One user LED is used as a status LED: reports the execution status of the example.
-
One user button is used to trigger events.
User LED ¶
By default, the user LED reports the execution status of the example. When a board offers multiple user LEDs, the example code uses:
-
Either the first one in the list.
-
Or gives preference to the green or blue LED over the red or orange LED.
|
Example status |
LED behavior and system state |
|---|---|
|
Success |
The LED remains turned on. The example scenario is done. The device is alive, no more action needed. |
|
Error |
The LED is flashing (50 ms on and 2 sec off). The device is running an error handler code. The variables and STM32 states are not reset and can be read with a debugger. |
|
Fault |
The LED is (tentatively) turned off. The device is running a fault handler. The STM32 state is unknown as a system fault has been encountered. |
Note
The LED behavior can be different for some examples (for example
hal_gpio_toggle
).
The specific LED behavior is documented in the README file of the example.
Using the pinout connections ¶
When an example generates signals on pins, the pinout connections are used to show the signal. The exact pinout scheme is documented in the README file of the example.
The preference list for pins selection is by priority order:
-
Arduino® UNO R3 connectors
-
STM32 Zio connectors
-
STM32 fanout connector
This means that the signals are evacuated on the Arduino® Uno V3 connectors whenever possible. An oscilloscope or a logical analyzer can be used to observe the signals on the pins of the STM32.
Additionally, some examples output a clock signal on the MCO [ 1 ] pin. You can connect this pin to an oscilloscope or a logical analyzer to observe the system clock or a peripheral clock.
Using the console ¶
Some examples generate applicative logs that are disabled by default.
These logs can be enabled by setting the
USE_TRACE
compiler switch to
1
.
Logs evacuation ¶
STLINK provides a virtual COM port interface allowing the host PC to communicate with the target STM32 through one UART. When enabled, the logs are sent over the UART instance connected to the virtual COM port of the STLINK mounted on the STM32 board.
The management of this UART is done by the
basic_stdio
utility.
Terminal settings ¶
A serial terminal emulator connected to the STLINK of the STM32 board is required to read the logs. We recommend using the Tera Term terminal emulator with these settings:
-
The serial terminal new-line transmit configuration must be set to LineFeed (n or LF) to allow copy-paste from UNIX® type text files. The selection of the local echo option makes copy-paste results visible on the console.
-
The serial port must be configured with the following settings:
-
COM port: COMx (where x is the number of the COM port assigned to the STLINK)
-
Baud rate: 115200
-
Data bits: 8
-
Parity: None
-
Stop bits: 1
-
Flow control: None
-
Using the debugger ¶
The example IDE projects are designed to be used with a debugger. The debug symbols are generated by default. The debugger can be used to set breakpoints, inspect variables, and step through the code.
Build profile ¶
The example projects are delivered with an optimized profile by default:
-
The compiler optimizations are enabled.
-
The step by step debugging can be impeded by these optimizations.
If you want to debug the example code step by step, you can use a
debug
build profile.
This build profile is not provided by default.
Refer to
Debug build profile
for more information on how to create a debug build profile.
System variables ¶
The variables declared in
main.c
are not required for the applicative use-case.
All the examples provide the
ExecStatus
variable that reports the current execution status of the example.
The
volatile
qualifier is set to this variable so that its content is always available in the debugger.