General debug tips ¶
Here are the typical points of attention to check in case of issue, from flashing the device to running the example code.
If you need to investigate further, this page also introduces:
-
A
debugbuild profile. -
A debug toolbox application note.
Flashing issues ¶
-
Try flashing using STM32CubeProgrammer.
-
Check the device configuration against the description in the AN2606 STM32 microcontroller system memory boot mode application note.
Startup issues ¶
-
Read the FLASH or RAM content using STM32CubeProgrammer to make sure the code you expect to run is loaded in the device.
-
Check the boot options of your device (boot pins, etc.) in the reference manual.
-
Try connecting to the board and use a debugger to spot any hard fault in the code (see the Fault exceptions page).
Issues to connect to the board ¶
-
Check if the firmware running on the target is forcing a low-power mode. The communication with ST-LINK is disabled when the board is in low-power mode.
-
Check if the target is secured or debug-disabled.
HAL timing issues ¶
-
Care must be taken when using
HAL_Delay(). This function provides an accurate delay (in milliseconds) based on a variable incremented in the SysTick ISR. This implies that ifHAL_Delay()is called from a peripheral ISR [ 1 ] process, then the SysTick interrupt must have higher priority (numerically lower) than the peripheral interrupt. Otherwise, the caller ISR process is blocked. To change the SysTick interrupt priority, use theHAL_NVIC_SetPriority()function. -
The example needs to ensure that the SysTick time base is always set to 1 millisecond to have correct HAL operation.
Debug build profile ¶
The STM32Cube Software Examples are provided with the debug symbols enabled, and the toolchain optimizations are enabled by default too. You can go further in terms of observability and debugging by updating these default settings.
Important
Do not use the settings provided in this section to estimate the performances of the system. This is only for observing and debugging the system, not for measuring its performances.
Observability ¶
Some examples offer an applicative log to follow the execution flow of the code.
This is disabled by default, but you can enable it by setting the
USE_TRACE
compiler switch to
1
.
These logs are not made to offer a full debug experience. Their primary purpose is to help you understand the example code and its execution flow.
Still, they allow you to observe when the execution flow deviates from the expected one.
To do so, you can check the nominal logs in the README file of the example (see
README
).
The pins of the STM32 can also be used to observe the signals on the board. See Using the pinout connections .
Step by step debugging ¶
When the toolchain optimizations are enabled, the step by step debugging can be impeded, and some variables may not be available in the debugger.
To debug the example code step by step, you can use a
debug
build profile.
In most examples, this build profile is not provided by default.
You can create it by following these steps:
-
Open the project in your IDE.
-
Create a new build profile named
debug. -
Set the compiler optimizations as indicated below:
-
For the GCC toolchain, set the optimization level to
-O0. Set the-g3flag to enable the maximum debug level.
-
For the IAR toolchain, set the optimization level to
LoworNone.
-
-
Build the project with this new profile.
-
Flash the device with the new binary.
-
Use the debugger to set breakpoints, inspect variables, and step through the code.
Warning
By disabling the compiler optimizations, you may significantly alter the binary it produces.
Performances
: the most demanding examples might not work with the
debug
build profile.
Code size : some examples might also not fit in the device memory, leading to a linker error. The stack size and heap size required by the example code can also increase. This can lead to a stack overflow or heap overflow unless you increase the appropriate settings in the linker script.
Memory layout : the placement of the code in memory changes. Updating some linker script sections and symbols might be required to ensure that the code operates correctly.
A
debug
build profile can be provided in some examples when it is complex to set up manually.
Debug toolbox ¶
Refer to the AN4989 STM32 microcontroller debug toolbox application note for further information about how to troubleshoot the problem.