STM32CubeMX2 STM32CubeMX2 STM32CubeMX2 Go to parent
/
  • latest
  • 1.0.0
  • English
ST Online Support

Table of contents

  • STM32CubeMX2 documentation
  • How to get started with STM32CubeMX2
  • How to start
    • System requirements
    • Installation
    • Uninstallation
    • Settings and preferences
    • Navigation and page structure
    • How to start from example projects
  • User manual
    • Home
    • Project settings
    • Clock
    • Pinout
    • Menu bar and left bar
    • Peripherals
    • DMA
    • NVIC
    • EXTI
    • Middleware and utilities
    • HW Parts
    • IDE project generation
    • Pack manager
    • Code preview
  • Command lines interface
  • How to
    • How to configure a clock
    • How to select an IDE and generate code
    • How to reserve a GPIO pin
    • How to access peripherals configuration
    • How to access hardware parts
    • How to access middleware & utilities
    • How to configure DMA
    • How to configure EXTI
    • How to configure NVIC
    • How is errors and conflicts propagation managed ?
  • Release Note
    • Release details
    • Release limitations
  • FAQ
  • Community

On this page

  • General interface
    • Top menu (1)
    • Tab bar (2)
    • Side bar (3)
    • Footer (4)
    • Main workspace (5)
  • How to use the split view
    • Split view button
    • Drag and drop
  • How to use the zoom
    • With the menu
    • With the shortcuts
  1. STM32CubeMX2 /
  2. How to start /
  3. Navigation and page structure

Navigation and page structure ¶

General interface ¶

Screenshot of the general interface of STM32CubeMX2

General interface of STM32CubeMX2 ¶

Some elements of the STM32CubeMX2 interface are common to most pages. These elements are the top menu, tab bar, sidebar, and footer.

Top menu (1) ¶

The top menu provides access to high-level features:

  • Project options: create, open, save, save as.

  • View options: Zoom In, Zoom Out, tab management.

  • Help: access documentation, software version, pack, and licenses.

Tab bar (2) ¶

../../../_images/TabBar.webp

Tab bar ¶

All STM32CubeMX2 pages open in dedicated tabs. Tab headers are displayed in this area. The following actions are available:

  • Close a tab: click the cross icon on the right of the tab header.

  • Display a tab: click the tab header.

  • Move a tab: click and hold the tab header, then drag it to another position.

Note

  • If too many tabs are open, some tab headers may not be visible. Use the mouse scroll wheel to navigate across tab headers.

  • A scrollbar will be displayed below the tab headers.

Side bar (3) ¶

../../../_images/SideBar.webp

Side bar with an opened project ¶

The sidebar is used to open new tabs in STM32CubeMX2. The available tabs are:

  1. Home: manage projects.

  2. Pinout: configure and manage microcontroller pin assignments and properties.

  3. Clock: configure and manage MCU clock.

  4. Peripherals: access peripheral configuration pages.

  5. Middleware: access middleware and utilities configuration pages.

  6. Parts: access parts configuration pages.

  7. Project settings: view project information, including generation settings.

  8. Generate IDE project: trigger IDE project generation.

  9. Pack manager: add, remove or update software packs.

  10. Settings: configure STM32CubeMX2 options.

Note

  • Except the Pack manager and the settings, all sidebar icons are disabled until a project is opened.

Footer (4) ¶

../../../_images/Footer.webp

Footer in a saved state & 11 notifications ¶

The footer displays different types of information:

  • Save status: on the left part of the footer, shows the current project’s save status. Possible statuses are “Saved” (all information saved) and “Click to save” (changes made since last save). Click “Click to save” to save the project.

  • Notifications: on the right part of the footer, there’s an icon used to access notifications. Click to display all notifications. The notifications are detailed in the next section.

Main workspace (5) ¶

The main workspace

  • is the place where the tabs will be displayed.

  • It’s possible to display several tab side by side, this will be detailed in the next chapter.

How to use the split view ¶

It is possible to display several tabs at a time. Tabs can also be resized to adapt to the current task.

There are two main ways to use this system: by using the Split view buttons in the tabs, or by using drag and drop.

Split view button ¶

There is a split view button in the top part of most pages. Use this button to create standard split views. Clicking this button splits the interface into two blocks of identical proportions .

There are several types of splits:

  • For left and right splits, the screen is split vertically.

  • For top and bottom splits, the screen is split horizontally.

Steps :

  1. Click the split view button.

  2. Select a type of split: left, right, top, or bottom.

  3. The current tab is displayed in the selected part.

Note

It is possible to select a type of split: left, right, top, or bottom.

Drag and drop ¶

It is also possible to use a split view by using drag and drop.

Steps :

  1. Click and hold the left button of your mouse while hovering over a tab header.

  2. A blue frame appears when you hover over the rest of the interface. The frame represents where the tab will appear.

  3. Drop the tab.

Note

  • Each tab can be resized vertically or horizontally.

How to use the zoom ¶

It’s possible to Zoom In (increase the size of the elements) or Zoom Out (decrease the size of the elements) in STM32CubeMX2.

There’s several way to do it:

With the menu ¶

To Zoom In or Out, it’s possible to use the menu.

../../../_images/Shortcut_Menu.webp

Zoom In and Out in the menu ¶

Click on ‘View’ in the menu, and:

  • Click on Zoom In to increase the size of the elements.

  • Click on Zoom Out to decrease the size of the elements.

With the shortcuts ¶

It’s also possible to Zoom In or Out with keyboards shortcuts. Depending on your keyboard configuration, you can use:

  • Click on Ctrl + + or Ctrl + = to increase the size of the elements.

  • Click on Ctrl + - or Ctrl + ) to decrease the size of the elements.

Previous
Settings and preferences
Next
How to start from example projects

© Copyright 2026, STMicroelectronics.

Built with Sphinx and the Shibuya theme.