Uninstallation

Uninstallation process

Uninstall on Windows

To uninstall STM32CubeMX2 using the uninstaller.exe utility:

  1. Navigate to the STM32CubeMX2 installation directory.

  2. Locate and run uninstaller.exe.

  3. Follow the on-screen instructions to complete the uninstallation. The process removes files and shortcut

Uninstallation process of STM32CubeMX2 on Windows

STM32CubeMX2 uninstaller start on Windows

STM32CubeMX2 uninstaller on Windows

STM32CubeMX2 uninstaller on Windows

Uninstall on Linux

To uninstall STM32CubeMX2 from Linux:

  • Open a terminal and navigate to the installation folder.

  • Enter ./uninstall to launch the uninstallation process.

  • Follow the on-screen instructions to complete the uninstallation.

STM32CubeMX2 uninstaller on Linux

STM32CubeMX2 uninstaller on Linux

Uninstall on MacOS

To uninstall STM32CubeMX2 from MacOS:

  • Open a terminal and navigate to the installation folder.

  • Enter ./uninstall to start the uninstallation process.

  • Follow the on-screen instructions to complete the uninstallation.

STM32CubeMX2 uninstaller on MacOS

STM32CubeMX2 uninstaller on MacOS

Uninstallation Status and Error Handling

If the uninstallation does not complete with 100% success, an uninstallation status summary is displayed.

Uninstallation status summary

Uninstallation status summary