Uninstallation

Uninstallation process

Uninstall on Windows

Follow these steps to uninstall STM32CubeMX2 from Windows :

  • In Windows settings, select Apps > Installed apps (1).

  • In the search bar, enter STM32CubeMX2 (2).

  • Select Uninstall next to STM32CubeMX2 (3).

Uninstallation process of STM32CubeMX2 on Windows

Uninstallation process of STM32CubeMX2 on Windows

  • Follow the on-screen instructions to complete the uninstallation. The process removes files and shortcuts:

    • Confirm the uninstallation by entering yes.

    • When the uninstallation completes, the message Uninstallation completed successfully appears. Press Enter to exit.

STM32CubeMX2 uninstaller on Windows

STM32CubeMX2 uninstaller on Windows

Note

If you use the uninstaller.exe from STM32CubeMX2 installation path, the tool is not completely removed. In these cases, reinstalling the software fails. To resolve this, open Control Panel from Windows Settings and perform a forced uninstallation.

Uninstall on Linux

To uninstall STM32CubeMX2 from Linux:

  • Open a terminal and navigate to the installation folder.

  • Enter ./uninstall to launch the uninstallation process.

  • Confirm the uninstallation by typing yes.

  • When the uninstallation is complete, the message “Uninstallation completed successfully” appears. Press Enter to exit.

STM32CubeMX2 uninstaller on Linux

STM32CubeMX2 uninstaller on Linux

Uninstall on MacOS

To uninstall STM32CubeMX2 from MacOS:

  • Open a terminal and navigate to the installation folder.

  • Enter ./uninstall to start the uninstallation process.

  • Confirm the uninstallation by entering yes.

  • When uninstallation completes, the message Uninstallation completed successfully appears. Press Enter to exit.

STM32CubeMX2 uninstaller on MacOS

STM32CubeMX2 uninstaller on MacOS