How to reserve a GPIO pin ¶
This guide provides a step-by-step procedure to set a GPIO pin in Reserved or Configured mode.
Step 1: Access the Pinout Tab ¶
In the Pinout tab, view the microcontroller pins.
Step 2a: Set a GPIO in Reserved mode ¶
2a-1: Reserve a GPIO Pin using the Detail view in the right of the screen ¶
Left-click the desired pin in the MCU package graphic view. In the detail view on the right of the screen, select GPIO. By default, the pin is set as Configured. Select Reserved. The pin color appears in light green.
Follow the animation to reserve a pin using the right menu.
Step 2b: Set a GPIO in Configured mode ¶
2b-1: Configure a GPIO Pin using the Detail view in the right of the screen ¶
Left-click the desired pin in the MCU package graphic view. In the detail view on the right of the screen, select GPIO. By default, the pin is set as Configured. If the pin has been previously Reserved, select Configured. The pin color appears in dark green.
Follow the animation to configure a pin using the right menu.
Troubleshooting ¶
If issues occur, consult the documentation or verify the pin configuration.