Constants ¶
-
SEQ_CONF_TASK_NBR
¶
-
Default number of tasks.
Default value is 32 (maximum), can be reduced by redefining it in seq_user_conf.h.
-
SEQ_CONF_PRIO_NBR
¶
-
Default value of priority levels.
The default priority value is 2, can be redefined in seq_user_conf.h.
-
SEQ_RFU
¶
-
Default value for unused parameter.
The default value for unused parameter is 0.
-
SEQ_DEFAULT
¶
-
Default value used to start the scheduling.
This informs the sequencer that all tasks registered must be considered
Note
This is a typical use in the application
while(1)
{
SEQ_Run(SEQ_DEFAULT);
}