Use-case code ¶
This section focuses on the code implementing the logic of the use-case. The configuration of the resources is covered in the Resources configuration section.
Overview ¶
The STM32Cube Software Examples demonstrate the STM32Cube APIs to use the STM32 microcontrollers through meaningful use-cases. Nevertheless, this code is not a product-level code, and is not intended to be used in production as is. The main priorities of the code are:
-
The code is meant to be educational and illustrative.
-
The code is structured to be easily reused and adapted.
-
The functional code is designed to be hardware-agnostic and toolchains agnostic.
The benefits you can get are:
-
Homogeneity: all examples are written the same way, with the same structure.
-
Education: the code is easy to read and understand, easy to link to the documentation.
-
Diversity: the code is designed to be reused and adapted across all STM32 series.
The use-case code is gathered in the
application/
folder of the project.
The main entry-points of the use-case are located in the
example.c
file.
The infrastructure of the example is centralized in the
main.c
file.
Infrastructure ¶
main.c
implements the infrastructure of the example. This code is the same for all examples, and is not intended to be modified.
It is only a basic infrastructure to schedule the functional code implemented in
example.c
and manage the termination of the example.
|
Function |
Description |
|---|---|
|
|
The main entry point of the example:
|
|
|
This function is entered when the example is successfully completed. It is used to report the success when the example terminates. For examples running in an infinite loop, this function is not implemented. |
|
|
This function is entered when an unrecoverable error occurs. It is used to report the error and to stop the execution of the example. This code is not supposed to be executed as all examples are proven to be functional. |
|
|
This function is entered when a fault occurs. It is used to report the fault and to stop the execution of the example. This code is not supposed to be executed as all examples are proven to be functional. |
|
Function |
Description |
|---|---|
|
|
The main entry point of the example:
|
|
|
This task, created in
|
|
|
This function is entered when an unrecoverable error occurs. It is used to report the error and to stop the execution of the example. This code is not supposed to be executed as all examples are proven to be functional. |
|
|
This function is entered when a fault occurs. It is used to report the fault and to stop the execution of the example. This code is not supposed to be executed as all examples are proven to be functional. |
Processing ¶
example.c
is the file implementing the example scenario logic with the HAL APIs:
-
Each scenario step is implemented here, and identified with a tag
########## Step X ########## -
The example code is structured in
app_xxx()functions andapp_process()is the functional part of the use-case. -
This code can leverage the
PRINTFservice to write applicative logs to the console. These logs are enabled by setting theUSE_TRACEcompiler switch to1.
This file also contains the user callbacks, and all local functions used to implement the example scenario.
Local functions are used to implement some helpers which are not at the core of the example scenario.
This keeps
app_process()
focused on the HAL calls, and the code snippets you may copy/paste in your own application.
The system and resources configuration code is not located in
example.c
. Refer to the
Resources configuration
page.
This is where the clocks, pins, and peripherals are configured.
The system initialization code is called from
main()
in
main.c
. The resources configuration services are called from
app_init()
in
example.c
.
Warning
The LL examples are not available yet.
Warning
The middleware examples are not available yet.
Warning
The part drivers examples are not available yet.
Warning
The utilities examples are not available yet.
Conventions ¶
Admonitions ¶
The comments use admonitions like
@user
tag to highlight possible modifications (see
How to port an example
).
Additional admonitions are used to highlight important information.
|
Type |
Description |
Example |
|---|---|---|
|
Attention |
Highlights a particularly important note that you must not overlook. |
Attention: the data rate you can reach depends on the resistors values. |
|
Warning |
Used when there may be negative consequences to consider if a recommendation is not obeyed. |
Warning: this variable must be 32-bit aligned. |
|
Note |
Notes have lesser importance. |
Note: no callback associated to this interrupt as it is used only to wake the system up. |
Naming rules ¶
In the example code, the naming rules aim at identifying easily:
-
the portions of code which are related to the example internal design.
-
the code snippets which can be re-used in your own application.
These rules apply to the code located in
example.c
.
|
Element |
Naming Rule |
Description |
|---|---|---|
|
Global Variables |
Global variables are written in
CamelCase
.
For example:
|
Global variables are required by the example code to operate and connect all services, but they are likely to be replaced by your own variables in your application. |
|
Local Variables |
Local variables are written in
snake_case
.
For example:
|
Local variables are used within the functions like
|
|
Main functions |
The major functions implementing the example are written in
snake_case
.
For example:
|
These functions implement the use-case with the functional APIs being demonstrated. They are of interest to provide code to be re-used in your own application. |
|
Helper functions |
Helper functions are written in
CamelCase
.
For example:
|
Helper functions are used to implement some services which are not at the core of the example scenario. This code is specific to the example and is not intended to be re-used in your own application. |
In a nutshell:
-
Elements written in CamelCase are specific to the example.
-
Elements written in snake_case can be of interest as code snippets for your own application.