HAL ETH How to Use ¶
- group ETH_How_To_Use
-
The HAL ETH driver can be used as follows: ¶
Initialization and Configuration: ¶
Declare a hal_eth_handle_t handle structure, for example:
hal_eth_handle_t heth;Set the ETH instance number to initialize in the heth handle.
Initialize the ETH low level resources:
Enable the Ethernet interface clock using
Initialize the related GPIO clocks.
Configure Ethernet pinout.
Configure Ethernet NVIC interrupt (in Interrupt mode).
Call HAL_ETH_Init() API to initialize the Ethernet peripheral (MAC, DMA, MTL and MDIO).
Declare a hal_eth_config_t configuration structure, for example:
hal_eth_config_t eth_config;Set the ETH global configuration parameters in the eth_config structure. Set the MAC Address. Select the MII/RMII/RGMII interface to use.
Call HAL_ETH_SetConfig() API to configure the Ethernet peripheral (MAC, MTL and DMA). Default MAC, MTL and DMA configurations are applied.
Channel Configuration: ¶
Configure and start each Rx and Tx Channel separately. The steps below apply to any Ethernet channel type (Rx or Tx).
All HAL ETH Channel APIs take the channel identifier argument ETH Tx and Rx channel identifiers
Configure and start the HAL ETH Tx/Rx Channel as follows:
Declare a hal_eth_tx_channel_config_t / hal_eth_rx_channel_config_t channel configuration structure, for example:
hal_eth_tx_channel_config_t / hal_eth_rx_channel_config_t ch_config;Call HAL_ETH_GetConfigTxChannel()/HAL_ETH_GetConfigRxChannel() API to retrieve selected Tx/Rx Channel parameters.
Update the ETH Tx/Rx Channel configuration parameters in the ch_config structure.
Set the maximum number of application buffers to be held in the DMA FIFO.
Update the Tx/Rx DMA Channel Configuration.
Update the Tx/Rx MTL Queue Configuration.
Update the Tx/Rx FIFO Event Configuration.
Call HAL_ETH_SetConfigTxChannel()/HAL_ETH_SetConfigRxChannel() API to configure the selected Tx/Rx Channel.
Retrieve memory allocation requirements to allocate memory for descriptors and application buffers to be used for reception and/or transmission.
Declare a hal_eth_channel_alloc_needs_t channel allocation info structure, for example:
hal_eth_channel_alloc_needs_t alloc_needs;Call HAL_ETH_GetChannelAllocNeeds() API to retrieve selected channel allocation information.
Use the allocation information to start the selected channel. The information includes:
The minimum memory size in bytes required by the driver for the selected channel.
The minimum address alignment for memory to be used by the driver.
Frame Reception: ¶
Ethernet data reception is asynchronous, so call the following API to start the listening mode for each initialized Rx Channel(s):
This API starts the MAC and DMA reception process. Configure the interrupt management mode and arguments.
Provide memory buffers to transfer the received frame data.
The ETH Rx Allocate Callback
p_rx_allocate_cbis called to allocate buffers for reception.
When data is received, the ETH Data Callback
p_data_cb(orHAL_ETH_DataCallback) is invoked if the channel is configured in interrupt mode.Call the HAL_ETH_ExecDataHandler() API to get the received data (in Thread execution mode).
The
p_rx_complete_cbandp_rx_allocate_cbcallbacks are called duringHAL_ETH_ExecDataHandlerexecution to notify about a received frame and request memory for the next frame reception.Call HAL_ETH_ExecDataHandler() API to retrieve received data at any time in the context of the application thread.
Communication with an external PHY device: ¶
HAL_ETH_MDIO_UpdateClockRange(): Update the MDIO clock range.
HAL_ETH_MDIO_SetOpAttributes(): Configure Ethernet MDIO command attributes.
HAL_ETH_MDIO_C22ReadData(): Read a register from an external PHY using Clause 22 method.
HAL_ETH_MDIO_C22WriteData(): Write data to an external PHY register using Clause 22 method.
HAL_ETH_MDIO_C45ReadData(): Read a register from an external PHY using Clause 45 method.
HAL_ETH_MDIO_C45WriteData(): Write data to an external PHY register using Clause 45 method.
HAL_ETH_MDIO_C45ReadDataRange(): Read a range of registers from an external PHY using Clause 45 method.
HAL_ETH_UpdateConfigLink(): Apply MAC link speed/duplex using hal_eth_link_config_t after link configuration change. It can result from auto-negotiation between PHYs, or from a manual or managed change of settings.
Advanced Ethernet Configurations: ¶
Configure the Ethernet MAC after ETH peripheral configuration is done: ¶
HAL_ETH_MAC_GetConfig(): Get MAC current configuration into hal_eth_mac_config_t.
HAL_ETH_MAC_SetConfig(): Set MAC configuration based on hal_eth_mac_config_t.
Configure the Ethernet DMA after ETH peripheral configuration is done: ¶
HAL_ETH_DMA_GetConfig(): Get DMA current configuration into hal_eth_dma_config_t.
HAL_ETH_DMA_SetConfig(): Set DMA configuration based on hal_eth_dma_config_t.
Configure the Ethernet MTL after ETH peripheral configuration is done: ¶
HAL_ETH_MTL_GetConfig(): Get MTL current configuration into hal_eth_mtl_config_t.
HAL_ETH_MTL_SetConfig(): Set MTL configuration based on hal_eth_mtl_config_t.
Configure ARP offload module after ETH peripheral configuration is done: ¶
HAL_ETH_EnableARPOffload(): Enable ARP offload.
HAL_ETH_DisableARPOffload(): Disable ARP offload.
HAL_ETH_IsEnabledARPOffload(): Check whether ARP offloading is enabled.
HAL_ETH_SetARPTargetIP(): Set the ARP Target IP address.
Configure MAC power down module: ¶
HAL_ETH_EnterPowerDownMode(): Enter the Power down mode.
HAL_ETH_ExitPowerDownMode(): Exit from the Power down mode.
HAL_ETH_SetRemoteWakeUpPcktFilter(): Set the Remote WakeUp filter.
Configure Energy Efficient Ethernet module: ¶
HAL_ETH_EnterLPIMode(): Enter the Low Power Idle (LPI) mode.
HAL_ETH_ExitLPIMode(): Exit the Low Power Idle (LPI) mode.
Callback registration: ¶
The ETH HAL driver supports two distinct sets of callbacks:
Mandatory callbacks Register these callbacks in the application. These callbacks are not delimited by the
USE_HAL_ETH_REGISTER_CALLBACKScompilation flag and have no weak default implementations.Optional callbacks These callbacks are delimited by the
USE_HAL_ETH_REGISTER_CALLBACKScompilation flag and are optional. When this flag is enabled, the integration can override the default weak implementations by registering its own callbacks.
By default, after a call to
HAL_ETH_Init()and while the state isHAL_ETH_STATE_INIT, all callbacks that provide weak default implementations are mapped to their corresponding weak functions (for exampleHAL_ETH_ErrorCallback(),HAL_ETH_WakeUpCallback()).Register or unregister callbacks only when the driver is in
HAL_ETH_STATE_CONFIGUREDstate.If
USE_HAL_ETH_REGISTER_CALLBACKSis set to0or not defined, the callback registration mechanism (for the callbacks guarded by this compile switch) is disabled and these callbacks remain bound to their weak implementations.Note: The following channel-related callbacks do not have weak default implementations and their registration is therefore mandatory:
Their implementation is not delimited by the
USE_HAL_ETH_REGISTER_CALLBACKScompilation flag. Register appropriate callbacks for each used channel.The HAL ETH driver provides the following callback registration functions:
HAL_ETH_RegisterChannelRxAllocateCallback(): Register RX buffer allocation callback for a specific channel (mandatory, no weak default).HAL_ETH_RegisterChannelRxCptCallback(): Register RX complete callback for a specific channel (mandatory, no weak default).HAL_ETH_RegisterChannelTxCptCallback(): Register TX complete callback for a specific channel (mandatory, no weak default).HAL_ETH_RegisterDataCallback(): Register data transfer/processing callback.HAL_ETH_RegisterWKUPCallback(): Register Ethernet wake-up (power management) callback.HAL_ETH_RegisterPMTCallback(): Register Power Management Trigger (PMT) callback.HAL_ETH_RegisterEEECallback(): Register Energy Efficient Ethernet (EEE) callback.HAL_ETH_RegisterErrorCallback(): Register error notification callback.HAL_ETH_RegisterEventCallback(): Register generic Ethernet event callback.HAL_ETH_RegisterCacheInvalidateCallback(): Register cache invalidate operation callback.HAL_ETH_RegisterCacheFlushCallback(): Register cache flush operation callback.HAL_ETH_RegisterChannelRxEventCallback(): Register generic RX event callback for a specific channel.HAL_ETH_RegisterChannelTxEventCallback(): Register generic TX event callback for a specific channel.
HAL ETH Driver State and Errors: ¶
Use HAL_ETH_GetState() function to return the global HAL ETH driver state.
Use HAL_ETH_GetChannelState() function to return the state of a specific ETH channel.
When enabled, use HAL_ETH_GetLastErrorCodes() to retrieve the last recorded ETH error codes.
If the compilation flag
USE_HAL_ETH_GET_LAST_ERRORSis set to 1, the functionHAL_ETH_GetLastErrorCodes()is available and allows the application to read back the last error codes recorded internally by the ETH driver.If
USE_HAL_ETH_GET_LAST_ERRORSis set to 0 or not defined, this function is not compiled and the last error history feature is not available.Note
Ensure buffer(s) respect memory allocation requirements (alignment) provided by HAL_ETH_GetChannelAllocNeeds() API call.
Note
Do not call any blocking service(s) while running in handler execution mode.
Note
Do not call HAL_ETH_ExecDataHandler() API in the Handler execution mode. This breaks driver behaviour. Implement a dedicated worker thread and trigger it to retrieve the received data (in Thread execution mode).