HAL OPAMP How to Use

group OPAMP_How_To_Use

OPAMP peripheral main features

OPAMP instances

The C5 device integrates three operational amplifiers: OPAMP1 & OPAMP2 & OPAMP3 (1) (1) OPAMP2 & OPAMP3 availability depends on the device

OPAMP configuration mode

The OPAMP provide(s) several exclusive configuration modes.

  • Standalone mode

  • Programmable Gain Amplifier (PGA) mode, with or without external filtering (A capacitor can be connected between OPAMP output and inverting input for filtering purpose, refer to reference manual)

  • Follower mode

OPAMP power mode

Each OPAMP instance can be configured in normal-power or low-power mode.

OPAMP speed mode

Each OPAMP instance can be configured in normal speed or high speed.

OPAMP calibration feature

The OPAMP provide(s) calibration capabilities.

  • Calibration aims at improving voltage offset accuracy

  • The OPAMP uses either factory calibration settings or user defined calibration settings (i.e. trimming mode).

  • The user trimming values can be figured out by calling calibration handled by HAL_OPAMP_Calibrate().

  • HAL_OPAMP_Calibrate()

    • Run automatically the calibration.

    • Enables the user trimming mode.

    • Updates the trimming registers values with fresh calibration results. The user might store the calibration results for latter usage (for example, monitoring the trimming based on temperature).

  • HAL_OPAMP_CalibrateParallel()

    • Run calibration in parallel for linked HAL OPAMP handles to speed up calibration processing time.

OPAMP configuration mode:

Standalone mode

  • OPAMP input and output are not internally connected. User can implement any circuitry using external components.

Follower mode

  • Inverting Input is connected internally, no external connection on inverting input.

Programmable Gain Amplifier (PGA) mode (Resistor feedback output)

  • The OPAMP output(s) is internally connected to resistor feedback.

  • OPAMP internal programmable gain is either x2, x4, x8 or x16. Two usages:

    • inverting output not used, only programmable gain.

    • inverting input used for external filtering coupled with programmable gain (ex: connected capacitor for low-pass filtering).

The OPAMPs inverting input

The OPAMPs inverting input can be selected according to the Reference Manual “OPAMP functional description” chapter.

The OPAMPs non-inverting input

The OPAMPs non-inverting input can be selected according to the Reference Manual “OPAMP functional description” chapter.

How to use HAL OPAMP module driver

The OPAMP HAL driver can be used as follows:

How to initialize the OPAMP low level resources:

How to start and stop the OPAMP instances:

Operational amplifier possible pin connections:

  • Cf Reference Manual

Note

clock is enabled inside HAL_OPAMP_Init() whenever USE_HAL_OPAMP_CLK_ENABLE_MODEL is not set to HAL_CLK_ENABLE_NO.