How to configure a clock ¶
Configuring the clock system is a fundamental step in STM32 microcontroller projects, as it determines the operating frequency and timing for the entire system. STM32CubeMX2 provides a graphical interface to configure clocks easily.
Here’s a detailed guide to identify and configure common clock scenarios:
Understanding STM32 Clock System Basics ¶
STM32 MCUs have multiple clock sources: - Fixed source/variable source and PLL to reach the max system frequency. - HSI (internal RC oscillator), HSE (external crystal), LSI, LSE, PLL, etc.
The clock tree controls CPU clock, peripheral clocks, and bus clocks (AHB, APB1, APB2).
Proper clock configuration ensures correct setup by detecting peripheral frequencies that exceed the maximum limit and suggests automatic fixes.
Clock Configuration access ¶
Open your project in STM32CubeMX2.
Go to the clock configuration tab to view the visual clock tree graph (similar to the reference manual).
Set values for clock elements such as dividers, multipliers, or sources to configure the clock.
Let STM32CubeMX2 validate the configuration and warn if frequencies are out of range.
Click the resolve clock issue button to get a solution for an error-free clock tree.
Revert to the default configuration if needed.
Enter a desired frequency; the system will find a valid configuration or notify if none exists.
Typical Clock Configuration Scenarios ¶
Scenario A: Use Internal Oscillator (HSI) as a system clock ¶
Use case: Simple applications without external crystal.
Steps:
In STM32CubeMX2, go to the Clock Configuration tab.
Select HSI as the clock source for the system clock (SYSCLK).
Configure System Clock if a higher frequency is needed.
Verify bus clocks (AHB, APB1, APB2) frequencies.
CubeMX will show if the configuration is valid.
Scenario B: Configure Peripheral Clocks (e.g., USB, ADC, Timers) ¶
Use case: Some peripherals need specific clock frequencies.
Steps:
In clock configuration, check peripheral clocks.
Configure dedicated dividers if needed.
Ensure that peripheral clock frequencies meet specifications.
Scenario C: Clock configuration with errors + resolve issue ¶
Introduce an error in the configuration.
Click on Resolve Clock Issues.
Scenario D: Clock source availability in RCC Config and Clock Tree ¶
The availability of a clock source in the Clock Tree depends on its activation state in RCC Config.
When a clock source is disabled in RCC Config:
The clock source cannot be edited in the Clock Tree view.
The clock source cannot be selected as a clock source in the Clock Tree view.
An information tooltip is displayed, indicating that the user must first enable the clock source in RCC.
When a clock source is enabled in RCC Config:
The clock source becomes editable in the Clock Tree view.
The clock source can be selected or left unused as a clock source in the Clock Tree.
When a clock source is later disabled in RCC Config after being used in the Clock Tree:
The clock source becomes disabled in the Clock Tree.
If it is currently selected as a clock source somewhere in the Clock Tree, such as for the system clock or a peripheral clock, it is highlighted in Error on the corresponding Mux.
Scenario E: Clock Reset to Default Value ¶
If you want to return to the default configuration, click on the Reset Clock button.
Scenario F: Clock Table ¶
You can use the table view to set your clock configuration.
Scenario G: lock/ unlock elements ¶
You can lock or unlock clock element.
Scenario H: Enable/ disable clock elements ¶
You can enable or disable clock elements in the RCC configuration tab. For example, enable HSE in the RCC configuration tab.
You can also enable or disable clock peripheral elements in their corresponding peripherals. For example, activate or deactivate DAC.
Tips and Best Practices ¶
Always check the maximum frequency specifications of your MCU.
Use external crystal (HSE) for applications needing precise timing.
Configure low-power oscillators (LSI, LSE) for RTC and watchdog.
Review peripheral clock requirements (USB, ADC, etc.).
Use STM32CubeMX2 validation feature to avoid invalid configurations.