Uninstallation ¶
Uninstallation process ¶
Uninstall on Windows ¶
To uninstall STM32CubeMX2 using the uninstaller.exe utility:
Navigate to the STM32CubeMX2 installation directory.
Locate and run uninstaller.exe.
Follow the on-screen instructions to complete the uninstallation. The process removes files and shortcut
STM32CubeMX2 uninstaller start on Windows ¶
STM32CubeMX2 uninstaller on Windows ¶
Uninstall on Linux ¶
To uninstall STM32CubeMX2 from Linux:
Open a terminal and navigate to the installation folder.
Enter ./uninstall to launch the uninstallation process.
Alternatively, you can start the uninstallation by double-clicking the uninstall.
Follow the on-screen instructions to complete the uninstallation.
STM32CubeMX2 uninstaller on Linux ¶
Uninstall on MacOS ¶
To uninstall STM32CubeMX2 from MacOS:
Open a terminal and navigate to the installation folder.
Enter ./uninstall to start the uninstallation process.
Alternatively, you can start the uninstallation by double-clicking the uninstall.
Follow the on-screen instructions to complete the uninstallation.
STM32CubeMX2 uninstaller on MacOS ¶
Uninstallation Status and Error Handling ¶
If the uninstallation does not complete with 100% success, an uninstallation status summary is displayed.
Uninstallation status summary ¶