HAL ICACHE How to Use

group ICACHE_How_To_Use

ICACHE Introduction

The Instruction Cache (ICACHE) is introduced on C-AHB code bus of Cortex-M33 processor to improve performance when fetching instruction and data from both internal and external memories. Some specific features like dual master ports, hit-under-miss, and critical-word-first refill policy, allow close to zero-wait-state performance in most use cases.

Main features

The main features of ICACHE are described below:

  • Bus interface

    • one 32-bit AHB slave port, the execution port (input from Cortex-M33 C-AHB code interface)

    • two AHB master ports: master1 and master2 ports (outputs to Fast and Slow buses of main AHB bus matrix, respectively)

    • one 32-bit AHB slave port for control (input from AHB peripherals interconnect, for ICACHE registers access)

  • Cache access

    • 0 wait-state on hits

    • Hit-under-miss capability: ability to serve processor requests (access to cached data) during an ongoing line refill due to a previous cache miss

    • Dual master access: feature used to decouple the traffic according to targeted memory. For example, the ICACHE assigns fast traffic (addressing flash and SRAM memories) to the AHB master1 port, and slow traffic (addressing external memories) to the AHB master2 port, thus preventing processor stalls on lines refills from external memories. This allows ISR (interrupt service routine) fetching on internal flash memory to take place in parallel with a cache line refill from external memories.

    • Minimal impact on interrupt latency, thanks to dual master

    • Optimal cache line refill thanks to WRAPw bursts of the size of the cache line (32-bit word size, w, aligned on cache line size)

    • n-way set-associative default configuration with possibility to configure as 1-way, means direct mapped

  • Memory address remap

    • Possibility to remap input address falling into up to four memory regions (used to remap aliased code in SRAM memories to the Code region, for execution from C-AHB code interface).

  • Replacement and refill

    • pLRU-t replacement policy (pseudo-least-recently-used, based on binary tree), algorithm with best complexity/performance balance

    • Critical-word-first refill policy, minimizing processor stalls

    • Possibility to configure burst type of AHB memory transaction for remapped regions: INCRw or WRAPw (size w aligned on cache line size)

  • Performance counters ICACHE implements two performance counters:

    • Hit monitor counter (32-bit)

    • Miss monitor counter (16-bit)

  • Error management

    • Possibility to detect an unexpected cacheable write access, to flag an error and optionally to raise an interrupt

  • Trust Zone security support

  • Maintenance operation

    • Cache invalidate: full cache invalidation, fast command, non interruptible.

How to use the HAL ICACHE driver

The HAL ICACHE driver can be used as follows:

Main use

  • Initialize the ICACHE according to the associated handle with HAL_ICACHE_Init() .

  • Set the configuration of the ICACHE to choose associativity mode with HAL_ICACHE_SetAssociativityMode() function (default is 2-ways).

  • Enable and disable up to four regions to remap input address from external memories to the internal Code region for execution with HAL_ICACHE_EnableRemapRegion() and HAL_ICACHE_DisableRemapRegion() functions.

  • Then start the ICACHE driver with HAL_ICACHE_Start() . You can enable the Error interrupt detection and allow to receive callbacks in case of cache function error.

  • Execute the ICACHE maintenance operations if necessary :

    • Use HAL_ICACHE_Invalidate() to invalidate the full cache content:

      • Cache content is lost, and reloaded when needed.

      • Used for complete invalidate of the ICACHE in case.

      • Blocking call until operation is done.

Monitoring performance

Interrupt Mode

HAL ICACHE Driver State