PLAY ¶
This section provides information about the migration APIs of the HAL PLAY driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL PLAY migration: list of applicable concepts
- HAL PLAY Typical use cases for migration
- HAL PLAY constants migration
- HAL PLAY macros migration
- HAL PLAY types migration
- HAL PLAY initialization and configuration functions migration
- HAL PLAY I/O operation functions migration
- HAL PLAY IRQ handler and callbacks functions migration
- HAL PLAY state and error functions migration
- HAL PLAY secure attributes settings functions migration
- HAL PLAY APIs listing for migration