XSPI ¶
This section provides information about the migration APIs of the HAL XSPI driver.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL XSPI migration: List of applicable concepts
- HAL XSPI typical use cases for migration
- HAL XSPI constants migration
- HAL XSPI macro migration
- HAL XSPI types migration
- HAL XSPI initialization and configuration functions migration
- HAL XSPI delay block functions migration
- HAL XSPI IO operation functions migration
- HAL XSPI state and control functions migration
- HAL XSPI callback functions migration
- HAL XSPI high-speed interface and calibration functions migration
- HAL XSPI APIs listing for migration