SD ¶
This section provides information about HAL SD driver migration from STM32 HAL1 to HAL2.
Before digging into the details of the HAL2 changes, it is important to understand the HAL2 breaking concepts explained in Breaking changes in concepts.
- HAL SD migration: List of applicable concepts
- HAL SD typical use cases for migration
- HAL SD constants migration
- HAL SD macros migration
- HAL SD types migration
- HAL SD initialization and configuration functions migration
- HAL SD I/O operation functions
- HAL SD peripheral control functions
- HAL SD interrupt handler and callbacks
- HAL SD state and error functions
- HAL SD APIs listing for migration