Resolve HAL1 detected references

This section demonstrates how to browse the detection log file and resolve the HAL1 API references by updating the application code to its HAL2 equivalent. The process is guided by the HAL1 to HAL2 migration documentation, ensuring a systematic and accurate transition.

Generated log

After the execution of the automatic detection script, a log folder is generated under HAL2_Migrator/hal1_detection_script_log.

Note

The HAL1 detection script generates an HTML log file that includes the user application code where HAL1 APIs are detected.


Example Image

Important

Open the generated log file to review the table of detected HAL1 references that require resolution. For each detected HAL API, begin the resolution process by clicking the corresponding documentation link.


Example Image

Example Image

Note

Each HAL1 API reference in the log is presented as a clickable link that directs the user to the corresponding section in the HAL1 to HAL2 migration documentation.

This feature enables quick navigation and efficient access to detailed migration guidance for each HAL1 API.


Example Image

Resolved project

After addressing all HAL1 references, the application code now compiles successfully without any errors or warnings.

Example Image

Example Image

See also: Alternative option using Stubbing