6. CMOX_CIPHER ¶
6.1. Key sizes for the cipher module ¶
- group CMOX_CIPHER_KEYSIZE
6.2. Cipher public method prototypes ¶
- group CMOX_CIPHER_PUBLIC_METHODS
-
Functions
-
cmox_cipher_retval_t
cmox_cipher_cleanup
(
cmox_cipher_handle_t
*
P_pThis
)
¶
-
Cleanup the cipher handle.
- Parameters :
-
P_pThis – Cipher handle to cleanup
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_init
(
cmox_cipher_handle_t
*
P_pThis
)
¶
-
Initialize the cipher handle for performing the specified algorithm.
Note
The cipher handle must be derived from an algorithm-specific handle using the correct constructor
- Parameters :
-
P_pThis – Cipher handle to initialize
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_setKey
(
cmox_cipher_handle_t
*
P_pThis
,
const
uint8_t
*
P_pKey
,
cmox_cipher_keyLen_t
P_keyLen
)
¶
-
Se the key to be used with the cipher algorithm.
Note
The XTS mode of operation requires a key with size double than the normal one (i.e. AES128-XTS will require a 32 bytes key, AES256-XTS will require a 64 bytes key and so on)
- Parameters :
-
P_pThis – Cipher handle to set
P_pKey – Buffer of bytes containing the key
P_keyLen – Len in bytes of the key
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_setIV
(
cmox_cipher_handle_t
*
P_pThis
,
const
uint8_t
*
P_pIv
,
size_t
P_ivLen
)
¶
-
Set the initialization vector/nonce to be used with the cipher algorithm.
- Parameters :
-
P_pThis – Cipher handle to set
P_pIv – Buffer of bytes containing the IV/nonce
P_ivLen – Size in bytes of the key
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_setTagLen
(
cmox_cipher_handle_t
*
P_pThis
,
size_t
P_tagLen
)
¶
-
Set the size of the tag for AEAD cipher.
Note
This function must be used only for AEAD ciphers. If used with other cipher, it won’t have any effects
Note
For ChaCha20-Poly1305 the tag size is fixed to 16 bytes, and this function has no effects
- Parameters :
-
P_pThis – Cipher handle to set
P_tagLen – Size in bytes of the tag
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_setPayloadLen
(
cmox_cipher_handle_t
*
P_pThis
,
size_t
P_totalPayloadLen
)
¶
-
Set the total payload size (only for CCM AEAD cipher).
Note
This function must be used for CCM ciphers. If used with other cipher, it won’t have any effects
- Parameters :
-
P_pThis – Cipher handle to set
P_totalPayloadLen – Size in bytes of the total payload
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_setADLen
(
cmox_cipher_handle_t
*
P_pThis
,
size_t
P_totalADLen
)
¶
-
Set the total authenticated data size (only for CCM AEAD cipher).
Note
This function must be used for CCM ciphers. If used with other cipher, it won’t have any effects
- Parameters :
-
P_pThis – Cipher handle to set
P_totalADLen – Size in bytes of the total authenticated data
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_appendAD
(
cmox_cipher_handle_t
*
P_pThis
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
)
¶
-
Append additional authenticated data to the cipher handle.
Note
This function must be used only for AEAD ciphers. If used with other cipher, it won’t have any effects
- Parameters :
-
P_pThis – Cipher handle where the authenticated data will be appended
P_pInput – Buffer of bytes containing the data to append
P_inputLen – Size in bytes of the data to append
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_append
(
cmox_cipher_handle_t
*
P_pThis
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
,
uint8_t
*
P_pOutput
,
size_t
*
P_pOutputLen
)
¶
-
Append part or the totality of the plaintext/ciphertext and return the corresponding ciphertext/plaintext.
Note
ECB and CFB modes of operation for AES and SM4 require that the input length for each append is multiple of the block size (i.e. 16 bytes)
Note
CBC mode of operation will apply CS2 ciphertext stealing in case the input length is greater than 16 bytes and not multiple of 16 bytes. After CS2 is applied, no more appends are allowed. Refer to NIST SP 800-38A Addendum.
Note
CTR, OFB, GCM and CCM modes of operation permits to have input not multiple of the block size (i.e. 16 bytes for AES and SM4), but after this no more further appends are allowed.
Note
For ChaCha20-Poly1305, this function can be called multiple times with P_inputLen multiple of 64 bytes. A single, last, call can be made with any value for P_inputLen.
Note
With the exception of KEYWRAP algorithm, the minimum size of P_pOutput buffer must be P_inputLen.
Note
For KEYWRAP mode, this function must be used to append the key to wrap, and must be done in a single call (no partial append of the key is supported). The P_pOutput buffer will contain the encrypted key AND the 8 bytes authentication tag. So the minimum size of this buffer must be P_inputLen + 8.
- Parameters :
-
P_pThis – Cipher handle to use for ciphering the data
P_pInput – Buffer of bytes containing the data to append
P_inputLen – Size in bytes of the data to append
P_pOutput – Buffer of bytes where there will be stored the encrypted or decrypted data
P_pOutputLen – Number of bytes that have been generated by the function. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_generateTag
(
cmox_cipher_handle_t
*
P_pThis
,
uint8_t
*
P_pTag
,
size_t
*
P_pTagLen
)
¶
-
Generate the authenticated tag in case the AEAD operation is an encryption.
Note
This function must be used only for AEAD ciphers in encryption mode. If used with other cipher, it won’t have any effects. If used with AEAD cipher in decryption mode, it will raise an error.
- Parameters :
-
P_pThis – Cipher handle used for encrypting the data
P_pTag – Buffer of bytes where there will be stored the generated tag
P_pTagLen – Number of bytes that have been processed by the function. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_verifyTag
(
cmox_cipher_handle_t
*
P_pThis
,
const
uint8_t
*
P_pTag
,
uint32_t
*
P_pFaultCheck
)
¶
-
Authenticate the processed data with the given tag.
Note
This function must be used only for AEAD ciphers in decryption mode. If used with other cipher, it won’t have any effects. If used with AEAD cipher in encryption mode, it will raise an error.
Note
P_pFaultCheck value, if the parameter is provided, MUST be checked to be equal to the retval, and both MUST be equal to the successful value. P_pFaultCheck MUST be checked only if the main result is successful, and has no relevance if the main result is not successful. Every comparison (both for the return value and for P_pFaultCheck) must be done against the success value, and not comparing the value with the failure value. Indeed, in presence of faults, especially P_pFaultCheck, could be a dirty value.
- Parameters :
-
P_pThis – Cipher used for decrypting the data
P_pTag – Buffer of bytes containing the tag to use for the verification
P_pFaultCheck – Optional value to check, together with the retval, to verify if some fault happened
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_encrypt
(
cmox_cipher_algo_t
P_algo
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
,
const
uint8_t
*
P_pKey
,
cmox_cipher_keyLen_t
P_keyLen
,
const
uint8_t
*
P_pIv
,
size_t
P_ivLen
,
uint8_t
*
P_pOutput
,
size_t
*
P_pOutputLen
)
¶
-
Encrypt or decrypt a message using a symmetric cipher.
Note
This single call function cannot be used for AEAD ciphers
- Parameters :
-
P_algo – Identifier of the cipher algorithm to use for the computation. This parameter can be one of the following:
CMOX_AESFAST_ECB_ENC_ALGO
CMOX_AESFAST_CBC_ENC_ALGO
CMOX_AESFAST_CTR_ENC_ALGO
CMOX_AESFAST_CFB_ENC_ALGO
CMOX_AESFAST_OFB_ENC_ALGO
CMOX_AESFAST_XTS_ENC_ALGO
CMOX_AESSMALL_ECB_ENC_ALGO
CMOX_AESSMALL_CBC_ENC_ALGO
CMOX_AESSMALL_CTR_ENC_ALGO
CMOX_AESSMALL_CFB_ENC_ALGO
CMOX_AESSMALL_OFB_ENC_ALGO
CMOX_AESSMALL_XTS_ENC_ALGO
CMOX_AESSMALL_KEYWRAP_ENC_ALGO
CMOX_SM4_ECB_ENC_ALGO
CMOX_SM4_CBC_ENC_ALGO
CMOX_SM4_CTR_ENC_ALGO
CMOX_SM4_CFB_ENC_ALGO
CMOX_SM4_OFB_ENC_ALGO
P_pInput – Buffer of bytes containing the data to encrypt or decrypt
P_inputLen – Length in bytes of the data to encrypt or decrypt
P_pKey – Buffer of bytes containing the key
P_keyLen – Length in bytes of the key
P_pIv – Buffer of bytes containing the IV/nonce
P_ivLen – Length in bytes of the key
P_pOutput – Buffer of bytes where there will be stored the encrypted or decrypted data
P_pOutputLen – Number of bytes that have been processed by the function. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_cipher_decrypt
(
cmox_cipher_algo_t
P_algo
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
,
const
uint8_t
*
P_pKey
,
cmox_cipher_keyLen_t
P_keyLen
,
const
uint8_t
*
P_pIv
,
size_t
P_ivLen
,
uint8_t
*
P_pOutput
,
size_t
*
P_pOutputLen
)
¶
-
Decrypt a message using a symmetric cipher.
Note
This single call function cannot be used for AEAD ciphers
- Parameters :
-
P_algo – Identifier of the cipher algorithm to use for the computation. This parameter can be one of the following:
CMOX_AESFAST_ECB_DEC_ALGO
CMOX_AESFAST_CBC_DEC_ALGO
CMOX_AESFAST_CTR_DEC_ALGO
CMOX_AESFAST_CFB_DEC_ALGO
CMOX_AESFAST_OFB_DEC_ALGO
CMOX_AESFAST_XTS_DEC_ALGO
CMOX_AESFAST_KEYWRAP_DEC_ALGO
CMOX_AESSMALL_ECB_DEC_ALGO
CMOX_AESSMALL_CBC_DEC_ALGO
CMOX_AESSMALL_CTR_DEC_ALGO
CMOX_AESSMALL_CFB_DEC_ALGO
CMOX_AESSMALL_OFB_DEC_ALGO
CMOX_AESSMALL_XTS_DEC_ALGO
CMOX_AESSMALL_KEYWRAP_DEC_ALGO
CMOX_SM4_ECB_DEC_ALGO
CMOX_SM4_CBC_DEC_ALGO
CMOX_SM4_CTR_DEC_ALGO
CMOX_SM4_CFB_DEC_ALGO
CMOX_SM4_OFB_DEC_ALGO
P_pInput – Buffer of bytes containing the data to encrypt or decrypt
P_inputLen – Length in bytes of the data to encrypt or decrypt
P_pKey – Buffer of bytes containing the key
P_keyLen – Length in bytes of the key
P_pIv – Buffer of bytes containing the IV/nonce
P_ivLen – Length in bytes of the key
P_pOutput – Buffer of bytes where there will be stored the decrypted data.
P_pOutputLen – Number of bytes that have been processed by the function. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_cipher_retval_t Cipher return value
-
cmox_cipher_retval_t
cmox_aead_encrypt
(
cmox_aead_algo_t
P_algo
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
,
size_t
P_tagLen
,
const
uint8_t
*
P_pKey
,
cmox_cipher_keyLen_t
P_keyLen
,
const
uint8_t
*
P_pIv
,
size_t
P_ivLen
,
const
uint8_t
*
P_pAddData
,
size_t
P_addDataLen
,
uint8_t
*
P_pOutput
,
size_t
*
P_pOutputLen
)
¶
-
Encrypt a message using AEAD cipher.
Note
This single call function can be used for AEAD ciphers only
- Parameters :
-
P_algo – Identifier of the AEAD cipher algorithm to use for the computation. This parameter can be one of the following:
CMOX_AESFAST_GCMFAST_ENC_ALGO
CMOX_AESFAST_GCMSMALL_ENC_ALGO
CMOX_AESSMALL_GCMFAST_ENC_ALGO
CMOX_AESSMALL_GCMSMALL_ENC_ALGO
CMOX_AESFAST_CCM_ENC_ALGO
CMOX_AESSMALL_CCM_ENC_ALGO
CMOX_CHACHAPOLY_ENC_ALGO
P_pInput – Buffer of bytes containing the data to encrypt
P_inputLen – Length in bytes of the data to encrypt
P_tagLen – Length in bytes of the authentication tag to append to the ciphertext
P_pKey – Buffer of bytes containing the key
P_keyLen – Length in bytes of the key
P_pIv – Buffer of bytes containing the IV/nonce
P_ivLen – Length in bytes of the key
P_pAddData – Buffer of bytes containing the additional data to be used for authentication
P_addDataLen – Length in bytes of the Additional data
P_pOutput – Buffer of bytes where there will be stored the encrypted and authenticated data (i.e. ciphertext + tag)
P_pOutputLen – Number of bytes that have been generated by the function. If correct, it will be the size of the encrypted and authenticated data (i.e. ciphertext + tag). It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_cipher_retval_t
cmox_aead_decrypt
(
cmox_aead_algo_t
P_algo
,
const
uint8_t
*
P_pInput
,
size_t
P_inputLen
,
size_t
P_tagLen
,
const
uint8_t
*
P_pKey
,
cmox_cipher_keyLen_t
P_keyLen
,
const
uint8_t
*
P_pIv
,
size_t
P_ivLen
,
const
uint8_t
*
P_pAddData
,
size_t
P_addDataLen
,
uint8_t
*
P_pOutput
,
size_t
*
P_pOutputLen
)
¶
-
Decrypt a message using AEAD cipher.
Note
This single call function can be used for AEAD ciphers only
- Parameters :
-
P_algo – Identifier of the AEAD cipher algorithm to use for the computation. This parameter can be one of the following:
CMOX_AESFAST_GCMFAST_DEC_ALGO
CMOX_AESFAST_GCMSMALL_DEC_ALGO
CMOX_AESSMALL_GCMFAST_DEC_ALGO
CMOX_AESSMALL_GCMSMALL_DEC_ALGO
CMOX_AESFAST_CCM_DEC_ALGO
CMOX_AESSMALL_CCM_DEC_ALGO
CMOX_CHACHAPOLY_DEC_ALGO
P_pInput – Buffer of bytes containing the authenticated and encrypted data (i.e. ciphertext + tag)
P_inputLen – Length in bytes of the the authenticated and encrypted data (i.e. ciphertext + tag)
P_tagLen – Length in bytes of the tag
P_pKey – Buffer of bytes containing the key
P_keyLen – Length in bytes of the key
P_pIv – Buffer of bytes containing the IV/nonce
P_ivLen – Length in bytes of the key
P_pAddData – Buffer of bytes containing the additional data to be used for authentication
P_addDataLen – Length in bytes of the Additional data
P_pOutput – Buffer of bytes where there will be stored the decrypted data
P_pOutputLen – Number of bytes that have been generated by the function. If correct, it will be the plaintext size. It is an optional parameter and can be set to NULL if not needed.
- Returns :
-
cmox_cipher_retval_t
cmox_cipher_cleanup
(
cmox_cipher_handle_t
*
P_pThis
)
¶
6.3. Cipher module public types ¶
- group CMOX_CIPHER_PUBLIC_TYPES
-
Typedefs
-
typedef
size_t
cmox_cipher_keyLen_t
¶
-
Type for specifying the key size for the cipher.
-
typedef
const
struct
cmox_cipher_vtableStruct_st
*
cmox_cipher_vtable_t
¶
-
Cipher Virtual Table.
This type specifies a pointer to the virtual table containing the methods for a particular algorithm (e.g. CBC or CHACHA20-POLY1305)
-
typedef
const
struct
cmox_cipher_algoStruct_st
*
cmox_cipher_algo_t
¶
-
Cipher algorithm type.
This type specifies the algorithm to use with the cipher module (e.g. CBC). The type is defined as a pointer to a structure, that contains the functions for the specific algorithm, defined in the library internally
-
typedef
const
struct
cmox_aead_algoStruct_st
*
cmox_aead_algo_t
¶
-
AEAD algorithm type.
This type specifies the AEAD algorithm to use with the cipher module (e.g. CCM or CHACHA20-POLY1305). The type is defined as a pointer to a structure, that contains the functions for the specific algorithm, defined in the library internally
-
struct
cmox_cipher_handle_t
¶
-
#include <cmox_cipher.h>
Cipher handle structure definition.
Public Members
-
cmox_cipher_vtable_t
table
¶
-
Cipher virtual table
-
uint32_t
internalState
¶
-
internal state of the cipher handle
-
cmox_cipher_vtable_t
table
¶
-
typedef
size_t
cmox_cipher_keyLen_t
¶