2. CMOX_HASH_RETVALS

2.1. Hash return values

group CMOX_HASH_RETVALS

Defines

CMOX_HASH_SUCCESS

Hash operation successfully performed.

CMOX_HASH_ERR_INTERNAL

Some error happens internally in the hash module.

CMOX_HASH_ERR_BAD_PARAMETER

One or more parameter has been wrongly passed to the function (e.g. pointer to NULL).

CMOX_HASH_ERR_BAD_OPERATION

Error on performing the operation (e.g. an operation has been called before initializing the handle).

CMOX_HASH_ERR_BAD_TAG_SIZE

The desired digest size is not supported by the hash algorithm.

Typedefs

typedef uint32_t cmox_hash_retval_t

Hash module return value type.