7. CMOX_EDDSA ¶
7.1. EDDSA public method prototypes ¶
- group CMOX_ECC_EDDSA_PUBLIC_METHODS
-
Functions
-
cmox_ecc_retval_t
cmox_eddsa_keyGen
(
cmox_ecc_handle_t
*
P_pEccCtx
,
const
cmox_ecc_impl_t
P_CurveParams
,
const
uint8_t
*
P_pRandom
,
size_t
P_RandomLen
,
uint8_t
*
P_pPrivKey
,
size_t
*
P_pPrivKeyLen
,
uint8_t
*
P_pPubKey
,
size_t
*
P_pPubKeyLen
)
-
Generate private and public keys to use with EDDSA.
Note
If P_RandomLen is not enough, an error is returned and P_pPrivKeyLen contains the minimum number of bytes of random to provide (and is also half the minimum length of P_pPrivKey), while P_pPubKeyLen contains the minimum length of P_pPubKey.
- Parameters :
-
P_pEccCtx – [in] Context for ECC operations
P_CurveParams – [in] Curve Parameters and point functions This parameter can be one of the following:
CMOX_ECC_ED25519_HIGHMEM
CMOX_ECC_ED25519_OPT_LOWMEM
CMOX_ECC_ED25519_OPT_HIGHMEM
CMOX_ECC_ED448_LOWMEM
CMOX_ECC_ED448_HIGHMEM
P_pRandom – [in] Buffer of random bytes
P_RandomLen – [in] Byte length of the random buffer
P_pPrivKey – [out] Buffer with the private key, whose first half will be the secret value and the second half will contain the public key
P_pPrivKeyLen – [out] Byte length of the private key
P_pPubKey – [out] Buffer with the public key
P_pPubKeyLen – [out] Byte length of the public key
- Return values :
-
CMOX_ECC_SUCCESS – Everything OK
CMOX_ECC_ERR_MATHCURVE_MISMATCH – Mathematical function set is not compatible with current ECC curve
CMOX_ECC_ERR_ALGOCURVE_MISMATCH – Curve is not compatible with current functionality
CMOX_ECC_ERR_BAD_PARAMETERS – Some NULL/wrong/empty parameter or Construct API not called
CMOX_ECC_ERR_WRONG_RANDOM – Random material too short or not valid for the functionality
CMOX_ECC_ERR_MEMORY_FAIL – Not enough memory
CMOX_ECC_ERR_INTERNAL – Something went wrong during internal computations (e.g. hash)
-
cmox_ecc_retval_t
cmox_eddsa_sign
(
cmox_ecc_handle_t
*
P_pEccCtx
,
const
cmox_ecc_impl_t
P_CurveParams
,
const
uint8_t
*
P_pPrivKey
,
size_t
P_PrivKeyLen
,
const
uint8_t
*
P_pMessage
,
size_t
P_MessageLen
,
uint8_t
*
P_pSignature
,
size_t
*
P_pSignatureLen
)
-
Generate a signature, using EDDSA.
- Parameters :
-
P_pEccCtx – [in] Context for ECC operations
P_CurveParams – [in] Curve Parameters and point functions This parameter can be one of the following:
CMOX_ECC_ED25519_HIGHMEM
CMOX_ECC_ED25519_OPT_LOWMEM
CMOX_ECC_ED25519_OPT_HIGHMEM
CMOX_ECC_ED448_LOWMEM
CMOX_ECC_ED448_HIGHMEM
P_pPrivKey – [in] Buffer with the private key, whose first half is the secret value and the second half contains the public key
P_PrivKeyLen – [in] Byte length of the private key
P_pMessage – [in] Buffer with the message to sign
P_MessageLen – [in] Byte length of the message
P_pSignature – [out] Buffer with the signature (concatenation of R and S)
P_pSignatureLen – [out] Byte length of the signature
- Return values :
-
CMOX_ECC_SUCCESS – Everything OK
CMOX_ECC_ERR_MATHCURVE_MISMATCH – Mathematical function set is not compatible with current ECC curve
CMOX_ECC_ERR_ALGOCURVE_MISMATCH – Curve is not compatible with current functionality
CMOX_ECC_ERR_BAD_PARAMETERS – Some NULL/wrong/empty parameter or Construct API not called
CMOX_ECC_ERR_MEMORY_FAIL – Not enough memory
CMOX_ECC_ERR_INTERNAL – Something went wrong during internal computations (e.g. hash)
-
cmox_ecc_retval_t
cmox_eddsa_verify
(
cmox_ecc_handle_t
*
P_pEccCtx
,
const
cmox_ecc_impl_t
P_CurveParams
,
const
uint8_t
*
P_pPubKey
,
size_t
P_PubKeyLen
,
const
uint8_t
*
P_pMessage
,
size_t
P_MessageLen
,
const
uint8_t
*
P_pSignature
,
size_t
P_SignatureLen
,
uint32_t
*
P_pFaultCheck
)
-
Verify a signature, using EDDSA.
Note
P_pFaultCheck value, if the parameter is provided, MUST be checked to be equal to the retval, and both MUST be equal to the successful value. P_pFaultCheck MUST be checked only if the main result is successful, and has no relevance if the main result is not successful. Every comparison (both for the return value and for P_pFaultCheck) must be done against the success value, and not comparing the value with the failure value. Indeed, in presence of faults, especially P_pFaultCheck, could be a dirty value.
- Parameters :
-
P_pEccCtx – [in] Context for ECC operations
P_CurveParams – [in] Curve Parameters and point functions This parameter can be one of the following:
CMOX_ECC_ED25519_HIGHMEM
CMOX_ECC_ED25519_OPT_LOWMEM
CMOX_ECC_ED25519_OPT_HIGHMEM
CMOX_ECC_ED448_LOWMEM
CMOX_ECC_ED448_HIGHMEM
P_pPubKey – [in] Buffer with the public key
P_PubKeyLen – [in] Byte length of the public key
P_pMessage – [in] Buffer with the message to verify
P_MessageLen – [in] Byte length of the message
P_pSignature – [in] Buffer with the signature (concatenation of R and S)
P_SignatureLen – [in] Byte length of the signature
P_pFaultCheck – [out] Optional value to check, together with the retval, to verify if some fault happened
- Return values :
-
CMOX_ECC_AUTH_SUCCESS – Signature verified
CMOX_ECC_AUTH_FAIL – Signature NOT verified
CMOX_ECC_ERR_MATHCURVE_MISMATCH – Mathematical function set is not compatible with current ECC curve
CMOX_ECC_ERR_ALGOCURVE_MISMATCH – Curve is not compatible with current functionality
CMOX_ECC_ERR_BAD_PARAMETERS – Some NULL/wrong/empty parameter or Construct API not called
CMOX_ECC_ERR_MEMORY_FAIL – Not enough memory
CMOX_ECC_ERR_INTERNAL – Something went wrong during internal computations (e.g. hash)
CMOX_ECC_ERR_INVALID_SIGNATURE – Input signature corrupted or not in the expected format
CMOX_ECC_ERR_INVALID_PUBKEY – Public key not in a valid format
-
cmox_ecc_retval_t
cmox_eddsa_keyGen
(
cmox_ecc_handle_t
*
P_pEccCtx
,
const
cmox_ecc_impl_t
P_CurveParams
,
const
uint8_t
*
P_pRandom
,
size_t
P_RandomLen
,
uint8_t
*
P_pPrivKey
,
size_t
*
P_pPrivKeyLen
,
uint8_t
*
P_pPubKey
,
size_t
*
P_pPubKeyLen
)