11. CMOX_KEYWRAP

11.1. KEYWRAP single-call algorithms

group CMOX_KEYWRAP_ALGO

Variables

const cmox_cipher_algo_t CMOX_AESSMALL_KEYWRAP_ENC_ALGO

Identifier of the KEYWRAP encryption using AES (small implementation) for single-call function (Defined internally).

const cmox_cipher_algo_t CMOX_AESSMALL_KEYWRAP_DEC_ALGO

Identifier of the KEYWRAP decryption using AES (small implementation) for single-call function (Defined internally).

const cmox_cipher_algo_t CMOX_AESFAST_KEYWRAP_ENC_ALGO

Identifier of the KEYWRAP encryption using AES (fast implementation) for single-call function (Defined internally).

const cmox_cipher_algo_t CMOX_AESFAST_KEYWRAP_DEC_ALGO

Identifier of the KEYWRAP decryption using AES (fast implementation) for single-call function (Defined internally).

11.2. KEYWRAP implementations

group CMOX_KEYWRAP_IMPL

Variables

const cmox_keywrap_impl_t CMOX_AESFAST_KEYWRAP_ENC

Implementation of KEYWRAP encryption using AES (fast implementation) (Defined internally).

const cmox_keywrap_impl_t CMOX_AESFAST_KEYWRAP_DEC

Implementation of KEYWRAP decryption using AES (fast implementation) (Defined internally).

const cmox_keywrap_impl_t CMOX_AESSMALL_KEYWRAP_ENC

Implementation of KEYWRAP encryption using AES (small implementation) (Defined internally).

const cmox_keywrap_impl_t CMOX_AESSMALL_KEYWRAP_DEC

Implementation of KEYWRAP decryption using AES (small implementation) (Defined internally).

11.3. KEYWRAP public macros

group CMOX_KEYWRAP_PUBLIC_MACROS

Defines

CMOX_KEYWRAP_TAG_LEN

Size in bytes of the keywrap tag.

11.4. KEYWRAP public method prototypes

group CMOX_KEYWRAP_PUBLIC_METHODS

Functions

cmox_cipher_handle_t * cmox_keywrap_construct ( cmox_keywrap_handle_t * P_pThis , cmox_keywrap_impl_t P_impl )

KEYWRAP constructor.

The function is used for specifying which block cipher algorithm to use in order to implement the KEYWRAP algorithm and if the algorithm will be used for encryption or decryption.

Parameters :
  • P_pThis – Pointer to the KEYWRAP handle to initialize

  • P_impl – Constant that specifies the implementation to use. This parameter can be one of the following values:

    • CMOX_AESFAST_KEYWRAP_ENC

    • CMOX_AESFAST_KEYWRAP_DEC

    • CMOX_AESSMALL_KEYWRAP_ENC

    • CMOX_AESSMALL_KEYWRAP_DEC

Returns :

cmox_cipher_handle_t* Pointer to a general cipher handle. This will be used by the general purpose cipher functions in order to perform the algorithm

11.5. KEYWRAP public types

group CMOX_KEYWRAP_PUBLIC_TYPES

Typedefs

typedef const struct cmox_keywrap_implStruct_st * cmox_keywrap_impl_t

KEYWRAP mode implementation.

This type specifies the used block cipher for the KEYWRAP construct and if the algorithm will be used for encryption or decryption. This type is defined as a pointer to a structure, that contains the functions needed for the specific implementation, defined in the library internally

struct cmox_keywrap_handle_t
#include <cmox_keywrap.h>

KEYWRAP handle structure definition.

Public Members

cmox_cipher_handle_t super

General cipher handle

cmox_blockcipher_handle_t blockCipher

Block cipher handle

uint32_t iv [ CMOX_CIPHER_BLOCK_SIZE ]

Buffer containing the Initialization Vector