1. CMOX_CMAC ¶
1.1. CMAC single-call algorithms ¶
- group CMOX_CMAC_ALGO
-
Variables
-
const
cmox_mac_algo_t
CMOX_CMAC_AESFAST_ALGO
-
Identifier of the CMAC using AES (fast implementation) for single-call function (Defined internally).
-
const
cmox_mac_algo_t
CMOX_CMAC_AESSMALL_ALGO
-
Identifier of the CMAC using AES (small implementation) for single-call function (Defined internally).
-
const
cmox_mac_algo_t
CMOX_CMAC_AESFAST_ALGO
1.2. CMAC implementations ¶
- group CMOX_CMAC_IMPL
-
Variables
-
const
cmox_cmac_impl_t
CMOX_CMAC_AESSMALL
-
Implementation of CMAC using AES (small implementation) (Defined internally).
-
const
cmox_cmac_impl_t
CMOX_CMAC_AESFAST
-
Implementation of CMAC using AES (fast implementation) (Defined internally).
-
const
cmox_cmac_impl_t
CMOX_CMAC_AESSMALL
1.3. CMAC public method prototypes ¶
- group CMOX_CMAC_PUBLIC_METHODS
-
Functions
-
cmox_mac_handle_t
*
cmox_cmac_construct
(
cmox_cmac_handle_t
*
P_pThis
,
cmox_cmac_impl_t
P_impl
)
-
CMAC constructor.
The function is used for specifying which block cipher algorithm to use in order to implement the CMAC algorithm.
- Parameters :
-
P_pThis – Pointer to the CMAC handle to initialize
P_impl – Constant that specifies the implementation to use. This parameter must be set with the following value:
CMOX_CMAC_AESFAST
CMOX_CMAC_AESSMALL
- Returns :
-
cmox_mac_handle_t* Pointer to a general MAC handle. This will be used by the general purpose MAC functions in order to perform the algorithm
-
cmox_mac_handle_t
*
cmox_cmac_construct
(
cmox_cmac_handle_t
*
P_pThis
,
cmox_cmac_impl_t
P_impl
)
1.4. CMAC public types ¶
- group CMOX_CMAC_PUBLIC_TYPES
-
Typedefs
-
typedef
const
struct
cmox_cmac_implStruct_st
*
cmox_cmac_impl_t
-
CMAC implementation.
This type specifies the used block cipher for the CMAC construct. This type is defined as a pointer to a structure, that contains the functions needed for the specific implementation, defined in the library internally
-
struct
cmox_cmac_handle_t
-
#include <cmox_cmac.h>
CMAC handle structure definition.
Public Members
-
cmox_mac_handle_t
super
-
General MAC handle
-
cmox_blockcipher_handle_t
blockCipher
-
Block cipher handle
-
uint32_t
iv
[
CMOX_CIPHER_BLOCK_SIZE
]
-
Buffer containing the Initialization Vector
-
uint8_t
temp_buffer
[
16
]
-
Temporary buffer to storing unprocessed data
-
uint32_t
unprocessed_bytes
-
Number of bytes in the temporary buffer
-
cmox_mac_handle_t
super
-
typedef
const
struct
cmox_cmac_implStruct_st
*
cmox_cmac_impl_t