1. CMOX_RSA

1.1. RSA public method prototypes

group CMOX_RSA_PUBLIC_METHODS

Functions

void cmox_rsa_construct ( cmox_rsa_handle_t * P_pRsaCtx , const cmox_math_funcs_t P_Math , const cmox_modexp_func_t P_Modexp , uint8_t * P_pBuf , size_t P_BufLen )

Mandatory function to set Low Level Mathematical Functions, and working memory buffer, for RSA.

Parameters :
  • P_pRsaCtx[inout] Context for RSA operations

  • P_Math[in] Structure pointer with the Low-level Mathematical functions This parameter can be one of the following:

    • CMOX_MATH_FUNCS_SMALL

    • CMOX_MATH_FUNCS_FAST

  • P_Modexp[in] Structure pointer with the Modular Exponentiation function This parameter can be one of the following:

    • CMOX_MODEXP_PUBLIC

    • CMOX_MODEXP_PRIVATE_LOWMEM

    • CMOX_MODEXP_PRIVATE_MIDMEM

    • CMOX_MODEXP_PRIVATE_HIGHMEM

  • P_pBuf[in] The preallocated static buffer that will be used

  • P_BufLen[in] The size in bytes of the P_pBuf buffer

void cmox_rsa_cleanup ( cmox_rsa_handle_t * P_pRsaCtx )

Clean the RSA context and the internal temporary buffer.

Parameters :

P_pRsaCtx [inout] Context for RSA operations

cmox_rsa_retval_t cmox_rsa_setKey ( cmox_rsa_key_t * P_pKey , const uint8_t * P_pModulus , size_t P_ModulusLen , const uint8_t * P_pExp , size_t P_ExpLen )

Set the key (public or private) in the key structure.

Parameters :
  • P_pKey[out] Key to set

  • P_pModulus[in] Modulus

  • P_ModulusLen[in] Modulus Length (in Bytes)

  • P_pExp[in] Exponent (private or public)

  • P_ExpLen[in] Exponent Length (in Bytes)

Return values :
  • CMOX_RSA_SUCCESS

  • CMOX_RSA_ERR_BAD_PARAMETER

cmox_rsa_retval_t cmox_rsa_setKeyCRT ( cmox_rsa_key_t * P_pPrivKey , size_t P_ModulusBitLen , const uint8_t * P_pExpP , size_t P_ExpPLen , const uint8_t * P_pExpQ , size_t P_ExpQLen , const uint8_t * P_pP , size_t P_PLen , const uint8_t * P_pQ , size_t P_QLen , const uint8_t * P_pIq , size_t P_IqLen )

Set the private CRT key in the key structure.

Parameters :
  • P_pPrivKey[out] Private Key to set

  • P_ModulusBitLen[in] Modulus Length (in bits)

  • P_pExpP[in] Secret exponent (mod P) dP

  • P_ExpPLen[in] dP Length (in Bytes)

  • P_pExpQ[in] Secret exponent (mod Q) dQ

  • P_ExpQLen[in] dQ Length (in Bytes)

  • P_pP[in] First secret prime P

  • P_PLen[in] P Length (in Bytes)

  • P_pQ[in] Second secret prime Q

  • P_QLen[in] Q Length (in Bytes)

  • P_pIq[in] Inverse of Q (mod P) invQ

  • P_IqLen[in] invQ Length (in Bytes)

Return values :
  • CMOX_RSA_SUCCESS

  • CMOX_RSA_ERR_BAD_PARAMETER

cmox_rsa_retval_t cmox_rsa_setKeyCRTwithFACM ( cmox_rsa_key_t * P_pPrivKey , size_t P_ModulusBitLen , const uint8_t * P_pExpP , size_t P_ExpPLen , const uint8_t * P_pExpQ , size_t P_ExpQLen , const uint8_t * P_pP , size_t P_PLen , const uint8_t * P_pQ , size_t P_QLen , const uint8_t * P_pIq , size_t P_IqLen , const uint8_t * P_pPubKey , size_t P_PubKeyLen )

Set the private CRT key in the key structure, enabling the Fault Attacks Countermeasure.

Note

This function enables the protection against the Bellcore attack for RSA-CRT computation. This countermeasure is useful to protect RSA-CRT using PKCS#1 v1.5 for Signature Creation. Indeed, PKCS#1 v2.2 Signature Creation is not vulnerable because of the presence of an input random, and Decryption processes (both for PKCS#1 v1.5 and v2.2) are not vulnerable because the plaintext is not returned if not correct (therefore not exploitable by an attacker).

Parameters :
  • P_pPrivKey[out] Private Key to set

  • P_ModulusBitLen[in] Modulus Length (in bits)

  • P_pExpP[in] Secret exponent (mod P) dP

  • P_ExpPLen[in] dP Length (in Bytes)

  • P_pExpQ[in] Secret exponent (mod Q) dQ

  • P_ExpQLen[in] dQ Length (in Bytes)

  • P_pP[in] First secret prime P

  • P_PLen[in] P Length (in Bytes)

  • P_pQ[in] Second secret prime Q

  • P_QLen[in] Q Length (in Bytes)

  • P_pIq[in] Inverse of Q (mod P) invQ

  • P_IqLen[in] invQ Length (in Bytes)

  • P_pPubKey[in] Public Key

  • P_PubKeyLen[in] Public Key Length (in Bytes)

Return values :
  • CMOX_RSA_SUCCESS

  • CMOX_RSA_ERR_BAD_PARAMETER