USBX Best practices ¶
Recommended ways to configure and use USBX with STM32
This section focuses on USBX middleware . It explains how to configure USBX for STM32 projects using:
-
STM32Cube + USBX,
-
RTOS or standalone (no OS) mode.
Global USBX configuration ¶
Core USBX options ¶
The following options are common to all STM32 USBX projects.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Define for host projects |
Enable USBX host stack. Use when STM32 is always USB host. |
|
|
Define for device projects |
Enable USBX device stack. Use when STM32 is always USB device. |
|
|
Define for no-OS (bare-metal) projects |
USBX runs without an RTOS. Used by STM32
|
|
|
Set to
|
Ensures buffers are properly aligned for USB/DMA. Required by ST USB drivers. |
|
|
Typically 100 |
USBX internal tick frequency (10 ms). Align with system tick where possible. |
|
|
Keep generous (for example 10000) |
Timeout for control transfers (enumeration, standard requests). |
|
|
Keep generous (for example 50000) |
Timeout for noncontrol transfers (bulk, interrupt, isochronous). |
Debug and safety options ¶
These options are part of USBX middleware and are supported in ST examples.
|
Macro |
Use in development |
Use in Production |
|---|---|---|
|
|
Enabled if you need USBX logs |
Typically disabled to reduce overhead |
|
|
Small-medium value (for example 256-512) |
0 or keep disabled log |
|
|
Enabled for bring-up and validation |
Disabled to avoid extra checks and code |
|
|
Enabled while validating integration |
Often disabled in size-optimized builds |
|
|
Enabled in early development |
Disabled once configuration is stable |
Name and alignment helpers:
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Optional; enable for strict alignment debug |
Typically disabled in production builds. |
|
|
Enable in footprint-focused projects |
USBX stores pointers to names instead of copies. Strings must be static or stay valid during USBX lifetime. |
Host-side USBX configuration ¶
Common host use cases with STM32 + USBX:
-
HID host (mouse, keyboard, joystick),
-
MSC host (USB flash drive),
-
CDC-ACM host (USB-to-serial),
-
audio or video host (streaming),
-
HUB host (multiple devices via hub).
Host build ¶
- For host projects:
-
-
Define
UX_HOST_SIDE_ONLY.
-
Core host ¶
These macros control host-side USBX internal resources.
|
Macro |
Typical values |
Usage |
|---|---|---|
|
|
1 |
Maximum host controllers. For STM32 USBX ports: usually 1. |
|
|
2 for single device; 3-4 with HUB |
Maximum USB devices under control (root + connected devices). |
|
|
2-4 |
Number of host classes. Examples: HCD + HID = 2; HCD + MSC = 2; HCD + HUB + HID + MSC = 4. |
|
|
1 (no HUB) to 4 (with HUB) |
Transaction translators. Mainly relevant when hubs are used. |
|
|
1-4 |
Number of root hub ports supported. Often 1 or 2 on STM32. |
Transfer descriptors and ED limits:
|
Macro |
Typical values |
Usage |
|---|---|---|
|
|
3-10 for basic; more for composite |
Endpoint descriptors. Must cover all active endpoints across connected devices. |
|
|
1-16 for most use cases |
Transfer descriptors. Start low and increase only in case of scheduling issues. |
|
|
1-2 for non-iso; higher for Audio/Video |
Isochronous transfer descriptors. Increase only for isochronous streaming classes. |
Host thread configuration (when using an RTOS) ¶
When USBX runs on RTOS, USBX uses internal host threads.
|
Macro |
Typical Range |
Notes |
|---|---|---|
|
|
512-1024 bytes |
Enumeration thread stack. Must handle parsing descriptors and class activation. |
|
|
128-1024 bytes |
HCD driver thread stack. Keep minimal but safe for your host driver logic. |
|
|
128-1024 bytes |
General USBX host thread stack, depends on enabled classes. |
ST’s USBX host examples use these macros in
ux_user.h
, and adjust them per class
(HID, MSC, CDC, etc.).
Device-side USBX configuration ¶
Common device use cases with STM32 + USBX:
-
HID device (mouse, keyboard, custom HID),
-
CDC-ACM device (virtual COM port),
-
MSC device (mass storage),
-
audio or video device,
-
Composite devices (for example CDC + MSC, HID + MSC).
Device build ¶
For device projects:
-
Define
UX_DEVICE_SIDE_ONLY.
Core device ¶
These macros control the device-side USBX internal objects.
|
Macro |
Typical values |
Usage |
|---|---|---|
|
|
1-2 |
Number of device classes registered. Use 1 for single-class devices (HID, MSC, CDC, Audio, Video). Use 2+ for composite devices. |
|
|
1-3 for simple classes |
Maximum number of interfaces. Match your USB descriptors (for example 1 for HID mouse, 2 for CDC-ACM). |
|
|
1 |
Number of LUNs for device MSC. Set to 1 for a single logical drive. |
Some ST ports also use:
|
Macro |
Typical values |
Usage |
|---|---|---|
|
|
Enough for all EPs + EP0 |
Maximum endpoint count. Keep minimal but cover all endpoints in your descriptors. |
|
|
Same order as
|
Internal interface limit, aligned with your descriptors. |
|
|
Enable only if used by port |
Used when the underlying ST USB driver exposes bidirectional endpoints. |
Standalone (no-OS) USBX ¶
USBX middleware provides a standalone mode used by ST “no-OS” examples.
Standalone mode basics ¶
|
Item |
Recommended usage |
Notes |
|---|---|---|
|
|
Define for bare-metal projects |
USBX runs without RTOS. The application calls USBX periodic functions explicitly. |
USBX Class best practices ¶
HID class (host + device) ¶
USBX middleware implements HID host and device classes, fully integrated with ST’s STM32 USB drivers.
Host HID ¶
Typical use: STM32 enumerates USB mouse, keyboard, joystick, gamepad, etc.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Enable only if OUT reports are used |
For example for LEDs or feature reports from host to device. |
|
|
Practical timeout (for example 10000) |
Controls how long the host waits for HID report transfers. |
|
|
Around 4096 bytes |
Buffer used to parse HID report descriptors. Increase only if complex devices fail. |
|
|
512-1024 |
Maximum number of HID usages. 512 is enough for simple mouse/keyboard. |
|
|
Enable for keyboard demos |
Provides key-change events rather than full key matrix each time. |
Device HID ¶
Typical use: STM32 as HID mouse, keyboard, or custom HID device.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
4-32 |
HID event buffer size. Increase for high-rate input devices. |
|
|
4-16 |
Maximum queued events before host reads them. |
|
|
Enable only if device uses OUT reports |
Required only when the HID device receives OUT reports from the host. |
|
|
Enable if application provides aligned persistent buffers |
Avoids internal copies for HID data, improving performance. |
MSC class (host + device) ¶
MSC Host (USB flash drive) ¶
USBX MSC host class is used in STM32 examples where MCU reads/writes USB sticks.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Minimal value that works well (for example 512-4096) |
Buffer used for MSC transfers. Increase if throughput is too low. |
|
|
Adjust to FileX + storage operations |
Set based on FileX usage and your application logic. |
|
|
1 |
Number of media supported. Set to 1 when only one USB flash is expected. |
|
|
512-4096 |
Max transfer chunk size, aligned with media sector size. |
|
|
Define if no FileX is used |
Use when you only need block-level access without a file system. |
|
|
1 |
Set to 1 for normal USB flash drives. |
MSC Device (USB mass storage device) ¶
USBX MSC device class allows STM32 to appear as a mass storage device.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
1 for single logical drive |
Increase only if multiple logical drives are exposed. |
|
|
Enable only if using MMC |
Keep disabled when media is not MMC-based. |
Integration hints (ST + USBX + FileX):
-
Use ST’s low-level media drivers (Flash, NOR, NAND, SD) plus FileX, then connect them to USBX MSC device/media callbacks.
CDC-ACM class ¶
CDC-ACM Device (virtual COM port) ¶
USBX middleware CDC-ACM device class is widely used on STM32 to emulate a COM port.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Enable for aligned, long-lived buffers |
Improves throughput by avoiding internal copies. Buffers must not be stack-based. |
|
|
Use when you need to temporarily disable transmissions |
For example during reconfiguration or error conditions. |
|
|
Enable if host expects ZLPs at end of transfers |
Automatically sends a zero-length packet when required by USB spec. |
-
Use 2 interfaces: one communication, one data.
-
For FS mode, endpoints use 64-byte max packet size.
-
Buffer sizes used should match target baud rate and latency requirements (often 256-512 bytes per direction is a good starting point).
CDC-ACM Host ¶
USBX CDC host class is used to connect STM32 to USB-to-serial adapters or other
CDC-ACM devices. Main tuning is done through host core parameters (
UX_MAX_DEVICES
,
UX_MAX_CLASSES
) and application-level buffer sizes.
Audio class (UAC) ¶
Audio Device ¶
USBX audio device class enables STM32 to act as a USB microphone, speaker or audio streaming endpoint.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Enable when using feedback endpoint |
Required for asynchronous isochronous modes using feedback. |
|
|
Small buffer (for example 64 bytes) |
Sufficient for feedback packets, keep minimal but safe. |
|
|
Enable only if audio interrupt endpoints are used |
Often disabled in simple audio streaming examples. |
-
Match endpoint configurations and sampling rates with ST USB audio examples.
-
Keep number of audio interfaces minimal (control + one stream where possible).
Audio Host ¶
USBX audio host class is used when STM32 receives or sends audio streams to a USB audio device.
-
Prefer HS USB when high audio bandwidth is required.
-
Keep advanced features (Audio 2.0, feedback, interrupt) disabled unless needed:
-
UX_HOST_CLASS_AUDIO_2_SUPPORT, -
UX_HOST_CLASS_AUDIO_FEEDBACK_SUPPORT, -
UX_HOST_CLASS_AUDIO_INTERRUPT_SUPPORT.
-
Video class (UVC) ¶
Video Device ¶
USBX video device class implements UVC-style streaming from STM32 to a host PC.
-
video requires large buffers:
-
For low footprint, keep resolution and frame rate low (e.g. 320x240, low FPS).
-
Use minimal buffering but enough to avoid frequent underruns.
-
Prefer HS USB for video.
-
Video Host ¶
USBX video host class is used when STM32 acts as video receiver from a UVC device.
|
Macro |
Recommended usage |
Notes |
|---|---|---|
|
|
Small but sufficient value (for example 1-8) |
Number of outstanding transfer requests used for streaming. Increase only to solve underrun/overrun issues. |
Prefer HS USB and ensure that host core limits (ED/TD/ISO TD counts) are large enough to cover all video endpoints.
Integration with STM32 and RTOS middleware ¶
RTOS integration ¶
-
Initialize the RTOS first.
-
Initialize USBX next, using ST-provided porting files in the STM32Cube package.
-
Create USBX host/device threads using:
-
RTOS APIs, or STM32 RTOS wrappers from the ST examples.
-
-
Ensure USBX threads have higher priority than non-critical tasks (for real-time USB).
FileX and storage ¶
When using FileX with USBX MSC:
-
Initialize FileX and low-level media drivers (ST drivers) before linking them to USBX MSC class.
Cache-MPU and STM32 USB drivers ¶
If your STM32 uses caches and/or MPU:
-
Follow ST’s USBX port notes about:
-
placing USB buffers in non-cacheable regions, or
-
performing appropriate cache clean/invalidate operations around USB transfers.
-
-
Honor
UX_ALIGN_MINand ST DMA alignment rules for all USB data buffers.
Checklist for a new USBX STM32 project ¶
-
Choose USB role:
-
Host → define
UX_HOST_SIDE_ONLY. -
Device → define
UX_DEVICE_SIDE_ONLY.
-
-
Select OS model:
-
With RTOS → configure USBX threads and stack sizes.
-
Standalone → define
UX_STANDALONEand rely on no-OS USBX examples.
-
-
Enable only the required USBX classes: * HID, MSC, CDC-ACM, Audio, Video, HUB, etc.
-
Set host and device limits based on your descriptors and topology:
-
Host:
UX_MAX_DEVICES,UX_MAX_HCD,UX_MAX_CLASSES,UX_MAX_TT,UX_MAX_ROOTHUB_PORT,UX_MAX_ED,UX_MAX_TD,UX_MAX_ISO_TD. -
Device:
UX_MAX_SLAVE_CLASS_DRIVER,UX_MAX_SLAVE_INTERFACES,UX_MAX_SLAVE_LUN,UX_MAX_DEVICE_ENDPOINTS,UX_MAX_DEVICE_INTERFACES.
-
USBX Footprint Summary ¶
|
Topic |
What was analyzed |
Main low-footprint strategy/observations |
|---|---|---|
|
Scope |
Examples/roles / OS |
Host HID, Device HID, Host MSC, Host & Device CDC-ACM,
HUB + MSC + HID, Host & Device Video, Host & Device Audio,
with RTOS and standalone (
|
|
Core utilities |
Generic USBX options |
Disable
|
|
Host core |
Host stack shape |
Define
|
|
Device core |
Device stack shape |
Define
|
|
HID footprint |
HID host & device |
Device: reduce
|
|
MSC footprint |
MSC host & device |
Host: reduce
|
|
CDC-ACM footprint |
CDC-ACM device |
Enable
|
|
audio footprint |
audio device |
Enable
|
|
video footprint |
video host & device |
Host: reduce
|
|
USBX pool sizing |
|
The tested value is the minimum that kept each example stable. When reusing in a different project, start from that value, add a safety margin, and stress-test with your own descriptors and traffic before reducing further. |
Links ¶
-
What is USBX? OverView
-
Getting started with USBX Getting started with USBX
-
USBX FAQ USBX FAQ
-
USBX Best practices and troubleshooting USBX Best practices