USBX Example list ¶
List of USBX device and host application examples provided by ST, with short descriptions
The STM32Cube MCU firmware packages deliver a rich set of USBX-based examples. They cover both USB device and USB host applications, showing how to integrate USBX with STM32 HAL, FreeRTOS, FileX.
USB device application examples ¶
|
Example |
Role / Class |
Short Description |
USBX examples Pack |
|---|---|---|---|
|
HID |
USB Device - HID (Human Interface Device) |
Implements standard HID devices. Demonstrates report descriptor setup and periodic report transmission. |
device_hid_mouse_freertos
device_hid_mouse_no_os
|
|
CDC ACM |
USB Device - CDC ACM (Communications Device Class - Abstract Control Model) |
STM32 enumerates as a USB virtual COM port. Shows full-duplex serial communication between the MCU and a PC terminal using the USBX CDC ACM device class. |
device_cdc_acm_uart_freertos |
|
CCID |
USB Device - CCID (Chip/Smart Card Interface Device) |
STM32 enumerates as a USB smart-card reader. Demonstrates CCID command exchange, slot management, and the integration of a smart-card style device service on top of USBX. |
device_ccid_freertos |
|
VIDEO |
USB Device - Video |
Streams MJPEG video data using the USBX video device class. Demonstrates USB video class integration with FreeRTOS. |
device_video_mjpeg_freertos |
USB host application examples ¶
|
Example |
Role / Class |
Short Description |
USBX examples Pack |
|---|---|---|---|
|
HID |
USB Host - HID (Human Interface Device) |
Enumerates and uses HID peripherals. Demonstrates interrupt IN transfers and HID report parsing. |
host_hid_no_os |
|
MSC |
USB Host - MSC (Mass Storage Class) |
STM32 acts as USB host and accesses USB flash drives. Demonstrates mounting a FileX volume, reading/writing files, and safe media removal. |
host_msc_freertos
host_msc_no_os
|
|
HUB |
USB Host - Hub |
Demonstrates USB hub support, managing multiple devices behind a hub (for example MSC + HID through a single upstream port). |
host_hub_msc_hid_freertos |
Links ¶
-
What is USBX? OverView