OverView

USBX is the USB middleware component of the Eclipse ThreadX RTOS family. It provides a comprehensive, high-performance, and portable USB host/device stack specifically optimized for resource-constrained embedded systems.

USBX supports a wide range of standard USB device and host classes (for example: MSC, CDC, HID, Audio, Video, Printer, and others), multiple endpoints, and all USB transfer types (control, bulk, interrupt, isochronous). The stack is written in ANSI C and is designed for straightforward porting across different 32-bit microcontroller architectures.

If you are new to USB, start with one question: what is the STM32 board expected to do on the cable?

  • In device mode , the STM32 behaves like a peripheral connected to a PC or another host. Examples include a virtual COM port, HID mouse, mass-storage device, or CCID smart-card reader.

  • In host mode , the STM32 behaves like the controller of the bus. It powers and enumerates external USB peripherals such as a flash drive, keyboard, mouse, or hub.

  • In dual-role designs , the product can use both paths, but the memory, power, descriptor, and instance-binding choices must stay consistent.

USBX decision guide for choosing USB device mode, host mode, or both

First decision point for a USBX project: select the USB role before choosing classes, controller settings, and generated code.

USBX on STM32 microcontrollers

On STM32 microcontrollers, USBX offers:

  • Seamless integration with the STM32Cube ecosystem

  • Support for all STM32 USB peripherals:

    • DRD Full-Speed (FS)

    • OTG Full-Speed (FS)

    • OTG High-Speed (HS)

  • Flexible operation with or without an RTOS :

    • Integrated with RTOS for fully multithreaded applications.

    • Usable in standalone bare-metal configurations (no RTOS).

Layered Architecture

The USBX architecture on STM32 is cleanly layered to improve clarity, reuse, and maintainability:

  • Application Layer User application code, high-level class behavior, data handling, and protocol logic specific to the end product.

  • USBX Core and Class Drivers USB protocol engine and standard class implementations (CDC, MSC, HID, etc.). This layer is independent from any specific STM32 device.

  • Low-Level Driver Layer STM32 USB drivers and board-support code that interface the USBX core with the underlying USB hardware peripheral.

This layered design simplifies USB application development, promotes portability across STM32 device families, and enables efficient reuse of existing USB solutions in new products.

Overall architecture

The high-level USBX architecture on STM32 can be summarized as:

  • Application code using USB class APIs (MSC, CDC, HID, etc.).

  • USBX core and class drivers managing enumeration, endpoints, and data transfers.

USBX overall block diagram

USBX overall block diagram

The reworked USBX middleware architecture preserves the same high-level software layering as the original implementation:

  • Controller Layer Interfaces directly with the hardware USB peripheral (device/host controllers, PHY, low-level drivers).

  • Core Processing Layer Manages core USB protocol operations such as enumeration, endpoint handling, transfers, and protocol state machines.

  • Class and Application Interface Layer Implements USB device and host classes (CDC, MSC, HID, etc.) and exposes interfaces used by the application layer.

  • Utility Layer for OS Portability Provides OS abstraction and common utilities to ensure portability of the USBX stack across different runtime environments (RTOS or bare metal).

USBX middleware folder structure

USBX folder structure

USBX folder structure

USBX root

Contains all USBX middleware files and subfolders.

Common

  • core - USB protocol core, state machines, utilities, macros, error codes.

  • usbx_device_class - device class implementations.

  • usbx_host_class - host class implementations.

  • usbx_host_controllers - generic EHCI/OHCI HCD drivers (not used on STM32 MCU).

  • usbx_pictbridge - PictBridge standard driver.

Ports

Platform-specific adaptation layer (FreeRTOS, other RTOSes, bare-metal).

Interfaces (STM32)

  • usbx_stm32_device_controllers - interface with STM32Cube USB PCD HAL.

  • usbx_stm32_host_controllers - interface with STM32Cube USB HCD HAL.

  • usbx_stm32_device_descriptors - runtime USB device descriptor builder.

Templates

Example USBX applications for different classes and modes.

Docs

Additional USBX documentation, revision history, features and dependencies.

USBX middleware architecture

Originally, the utility layer supported only ThreadX RTOS , and its OS-specific utility files were located under the common/core folder.

USBX middleware utility for Eclipse ThreadX

Eclipse ThreadX USBX middleware utility

The main rework consists of making this utility layer RTOS-agnostic , ensuring portability of USBX across different operating systems, especially FreeRTOS .

The new OS-agnostic utility layer:

  • Provides the essential services and abstractions required by USBX (threads, synchronization, memory, timing, etc.).

  • Allows integration with various RTOS environments.

  • Preserves compatibility with bare metal (no RTOS) configurations.

The RTOS-agnostic utility files are now organized under a ports directory, with a dedicated subfolder for each supported operating system or execution environment. For example:

  • ports/FreeRTOS - utilities and OS abstraction for FreeRTOS.

  • ports/generic - generic / bare-metal configuration (no RTOS).