User interface

Visual Studio Code (VS Code) features a user-friendly interface that improves productivity and supports efficient development. The following are key components of the VS Code user interface:

  • Activity Bar: Located on the far left, the Activity Bar enables switching between different views, such as Explorer, Search, Source Control, Run and Debug, and Extensions.

  • Side Bar: The Side Bar displays various views and panels based on the activity selected in the Activity Bar. For example, the Explorer view displayes project files and folders.

  • Editor: The central area for writing and editing code. VS Code supports multiple editors side by side, allowing work on different files at the same time.

  • Status Bar: Located at the bottom, the Status Bar provides information about the current state of VS Code, such as the Git branch, file encoding, and line endings.

  • Command Palette: Accessible by pressing [Ctrl + Shift + P], the Command Palette provides quick access to many commands and features in VS Code. It is a powerful tool for executing commands without using menus.

  • Panels: Panels are located at the bottom of the editor area and display tools such as the Terminal, Output, Debug Console, and Problems panel.

  • Tabs: Tabs at the top of the editor allow quick switching between open files. Tabs can be dragged and dropped to reorder them or opened in new editor groups.

Understanding these components of the user interface helps users navigate and use Visual Studio Code more effectively, improving the development experience.

For more detailed information, see Visual Studio Code User Interface Documentation.