User interface

Visual Studio Code (VS Code) is designed with a user-friendly interface that enhances productivity and makes development more efficient. Here are some key components of the VS Code user interface:

  • Activity Bar : Located on the far left, the Activity Bar allows you to switch between different views such as Explorer, Search, Source Control, Run and Debug, and Extensions.

  • Side Bar : The Side Bar displays different views and panels depending on the activity selected in the Activity Bar. For example, the Explorer view shows your project files and folders.

  • Editor : The central area where you write and edit your code. VS Code supports multiple editors side by side, allowing you to work on different files simultaneously.

  • Status Bar : Located at the bottom, the Status Bar provides information about the current state of VS Code, such as Git branch, file encoding, line endings, and more.

  • Command Palette : Accessible via Ctrl + Shift + P , the Command Palette provides quick access to many commands and features in VS Code. It is a powerful tool for executing commands without navigating through menus.

  • Panels : Panels are located at the bottom of the editor area and can display various tools like the Terminal, Output, Debug Console, and Problems panel.

  • Tabs : Tabs at the top of the editor allow you to switch between open files quickly. You can also drag and drop tabs to reorder them or open them in new editor groups.

Understanding these components of the user interface will help you navigate and utilize Visual Studio Code more effectively, enhancing your development experience.

For more detailed information, visit the Visual Studio Code User Interface Documentation .