Firmware security and integrity ¶
Security and integrity controls are required for reliable firmware lifecycle management. This chapter describes practical controls for STM32 projects using STM32CubeIDE for Visual Studio Code.
This chapter focuses on:
Protecting release artifacts from unauthorized modification
Verifying firmware identity before activation
Reducing rollback and debug-access risks in production
Defining validation evidence for release approval
Threat model and scope ¶
Define a security scope before implementation. Security controls must match the product deployment model and threat surface.
Typical threat classes are:
Unauthorized firmware replacement
Downgrade to a vulnerable firmware version
Extraction of sensitive data through debug interfaces
Tampering during transfer or storage
Document assumptions explicitly:
Physical access level to the target hardware
Network exposure of update transport
Required regulatory and product constraints
Note
This chapter defines implementation patterns, not product certification claims.
Secure build and artifact controls ¶
Security starts in the build pipeline. A trusted update process is not possible with untrusted artifacts.
Use these controls in STM32CubeIDE for Visual Studio Code workflows:
Build release artifacts from a tagged source revision.
Record artifact hashes for
.elf,.hex, and.binoutputs.Keep build and programming tasks under version control in
.vscode/tasks.json.Record bundle and toolchain baseline used for the release build.
For artifact and task context, see Build and API manual.
Integrity verification patterns ¶
An update image must be verified before activation.
Common verification layers are:
Transport integrity check
Image hash verification
Signature verification when the product architecture supports it
Minimum activation policy:
Validate image format and size constraints.
Validate image integrity metadata.
Reject activation on any verification failure.
Keep previous confirmed image available when product architecture allows it.
Store verification result codes in logs that are accessible during support and failure analysis.
Anti-rollback version policy ¶
Define a firmware version policy that blocks vulnerable downgrades.
Policy elements:
Monotonic version identifier
Explicit compatibility rules between bootloader and application
Allowed downgrade exceptions for service operations
Implementation guidance:
Compare incoming version against stored minimum accepted version.
Reject unauthorized downgrade attempts.
Record downgrade rejection events for diagnostics.
Caution
Downgrade policy must be tested with real recovery scenarios before production rollout.
Debug access in production ¶
Debug access policy is part of the security model.
For production targets:
Define when debug access is disabled, restricted, or service-controlled.
Separate development and production debug configurations in
launch.json.Require explicit service procedure for any temporary debug enablement.
For development targets:
Keep full debug visibility for root-cause analysis.
Avoid reusing development debug settings in production images.
For debug workflow details, see Debug.
Key and secret handling basics ¶
If the product uses cryptographic verification, key handling must be controlled throughout the lifecycle.
Baseline practices:
Keep private signing keys outside source repositories.
Use environment or secure-service injection for signing operations.
Restrict signing permissions to approved release roles.
Rotate keys based on product policy and incident response requirements.
Do not store long-term secrets in project files, task files, or launch configurations.
Security validation checklist ¶
Before release approval, verify at least the following on target hardware:
Artifact hash matches release manifest.
Invalid image is rejected before activation.
Version rollback policy behaves as specified.
Production debug access policy is enforced.
Recovery path works after interrupted update simulation.
Release evidence should include:
Build and hash logs
Verification and activation logs
Security test verdict summary
Incident response readiness ¶
Prepare response procedures before field deployment.
Response plan should define:
How to identify affected firmware versions
How to block vulnerable update paths
How to deploy corrected firmware safely
How to collect diagnostics without expanding exposure
Maintain a tested rollback or recovery path for emergency updates.
Recommended project practices ¶
To keep security controls stable across product iterations:
Review threat model at each major release
Keep security requirements in product-level specifications
Validate secure update behavior in continuous integration gates
Re-run security regression tests after toolchain or bundle upgrades