First project creation

There are several ways to get started. Go to the chapter that best matches your use case:

Quick path selection

Starting point

Recommended path

Expected result

First check

No existing project

Create empty project

New CMake project is generated

Project folder opens in Visual Studio Code

Existing STM32CubeMX project

Import STM32CubeMX project

Existing configuration is imported

.ioc and generated files are detected

STM32Cube firmware example

Import example project

Example is extracted and configured

Build output is generated without setup errors

Use the path above first, then continue with the related procedure.

Creating an empty project gives developers full control and flexibility. Developers can customize the environment, avoid unnecessary components, and optimize workflows. This approach is ideal for learning, experimentation, and creating scalable, maintainable code. It also fosters a deeper understanding of project setup.

Importing a project from STM32CubeMX provides a quick and efficient way to start development with preconfigured peripherals, clock settings, and middleware. This method ensures best practices, enhances code reliability, and integrates seamlessly with STM32CubeIDE for Visual Studio Code to simplify debugging and project management.

Importing an example project from STM32CubeMX into Visual Studio Code provides a quick start with preconfigured settings, peripherals, and middleware. These projects save time, follow best practices, and serve as valuable learning tools. Developers can focus on application-specific features and accelerate development.

Create empty project

Step 1: Initiate project creation

First, open the STM32CubeIDE for Visual Studio Code extension by clicking the STM32CubeIDE for VS Code butterfly icon in the Activity Bar. Click the “Create empty project” button to start setting up a new project.

Screenshot showing the “Create empty project” button in the STM32CubeIDE for Visual Studio Code extension.

Step 2: Name the project

Enter a name for the project.

Step 3: Select project type

Choose whether the project targets a device or a board . This selection determines the specific hardware configuration for the project.

Step 4: Choose the target

Select the correct target from the drop-down menu. This configures the project for the specific STM32 device or board.

Screenshot displaying the drop-down menu for selecting the device or board name in the STM32CubeIDE for Visual Studio Code extension.

Note

The list is data-driven. The MCUs and boards shown are based on CMSIS-PACK PDSC files.

Step 5: Define project location

Select the directory where the project files will be saved.

Step 6: Select toolchain

Select the toolchain to use. The toolchain determines the set of tools and libraries for building and managing the project. By default, GCC is selected. After selecting the toolchain, click “Create project” to continue.

Screenshot of the final settings window where you select the toolchain and project location in the STM32CubeIDE for Visual Studio Code extension.

Step 7: Open project
Visual Studio Code prompts you to choose how to open the new project. The options are:
  • Open in this window. Reuses the current instance of Visual Studio Code.

  • Open new window. Opens a new instance of Visual Studio Code.

  • Add to workspace. Adds the project to the current instance of Visual Studio Code (multiple projects in parallel).

Screenshot showing the options for opening the new project in VS Code: Open in this window, Open new window, or Add to workspace.

Step 8: Select CMake preset

Select the CMake preset (Debug or Release) and build configuration for the project.

Step 9: Run CMake configure

After selecting the CMake preset, CMake runs the configure step on the active preset context (for example, Debug). This process generates the necessary build files and creates a new folder in build/$CMakePresetName.

By following these steps, you create an empty project in the STM32CubeIDE for Visual Studio Code extension, ready for development.

Import STM32CubeMX project

Step 1: Initiate project creation

Open STM32CubeMX standalone and click File > New Project to start setting up a new project.

Step 2: Choose the target

Choose whether the project targets an MCU/MPU or a board. After selecting the device, click Start Project .

Step 3: Select toolchain

Enter a project name and select CMake as the toolchain/IDE.

Screenshot of the selection of a project name as well as showing the selection of CMake as the toolchain.

To open in Visual Studio Code, see the Open in VS Code guide.

Import example project

Tip

This operation is also available through the command-line interface. For more information, use the command:

$ cube project_extractor --help
Step 1: Initiate project creation

Go to the STM32Cube key actions menu and select Import STM32Cube example(s) .

Step 2: Choose the folder

Go to the root folder of the firmware pack for the board or MCU and click Select .

Step 3: Open the example selector

A list of the available examples appears in the example selector window. Select the example to import. In the Action column, click the icon to import the project.

Step 4: Select folder for extraction

Select the folder where the project is exported for use in Visual Studio Code.

Open in VS Code

Step 1: Open folder

Open the newly created project in Visual Studio Code. Go to File and select Open Folder… .

Screenshot showing the operation in VS Code of going to File and selecting Open Folder

Step 2: Select configure preset

After opening the project, select a configure preset . In this guide, “Debug” is selected.

Screenshot of the options available when selecting a configure preset with Debug highlighted.

Step 3: Setup STM32Cube project

To make CMake aware of the project, go to the STM32CubeIDE for Visual Studio Code extension and click Discover STM32Cube project .

Screenshot of the options Setup STM32Cube project after selecting the STM32CubeIDE for Visual Studio Code extension.

Step 4: Project Setup

Select the board or device, toolchain and project to target. Because this guide uses a single-core board, select the main project. After making selections, click Save and close .

Screenshot of the options to select the board/device, toolchain, and project.

The output log should look similar to the following:

Screenshot showing the output log of an expected project import.

If the output log matches, the project is ready to build. Refer to the Build guide for instructions.